Other Parts Discussed in Thread: DP83640, HALCOGEN
Hi all,
I have a couple of questions after looking into the available options for an evaluation module; primarily for testing the DP83640 chip.
Having gone through the TI website I have found the following, and please do correct me if I am wrong:
(1) The DP83640T Evaluation Demo Board ( www.ti.com/.../dp83640t-evk ), which can be controlled directly via a host PC and with no MAC functionality or anything else. Just the chip and a USB cable with supporting software to control it directly.
(2) The TMS570LC43x Hercules Development Kit ( www.ti.com/.../TMDX570LC43HDK ) and RM57L Hercules Development Kit ( www.ti.com/.../TMDXRM57LHDK ) ,that are pretty much identical. These come with a processor with MAC functionality on which you can develop your own code. My question is, what resources are available to develop the said code, probably in code composer studio ? I have found the relevant libraries in the following link ( www.ti.com/.../snlu049 ) but I am guessing this is more to develop scripts when using (1) above.
(3) The Launch Pad version of (2) above but with far less connectivity options; with either of the Hercules processors (www.ti.com/.../launchxl2-rm57l ). Same as above really, what options are there for code development ?
Any information would be greatly appreciated. Thank you in advance for your time.
Regards,
Evripidis