Other Parts Discussed in Thread: TMS570LS1227, HALCOGEN
Hey guys,
i have an TMS570LS1227 HDK and won't to run my code on it. But i have problems connection to the onboard XDS100v2 Debug Probe.
On an other pc it is working like plug and play but for me not.
So my setup is Windows 10 x64 running on my Mac in VMWare Fusion. I had already a TMS Launchpad with an XDS110 Debug Probe onboard, that config was working without problem.
Now when i setup the target like that XDS 100v2 / TMS1227 and try test connection it gives me back the following:
[Start: Texas Instruments XDS100v2 USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\MORITZ~1\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Dec 9 2015'.
The library build time was '20:05:50'.
The library package version is '6.0.83.1'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-150' (0xffffff6a).
The title is 'SC_ERR_FTDI_FAIL'.
The explanation is:
One of the FTDI driver functions used during
configuration returned a invalid status or an error.
[End: Texas Instruments XDS100v2 USB Debug Probe]
I have already fresh installed windows with code composer and have no idea what the problem is.
The XDS100v2 Debug probe gehts right recognized in the device manager.
Would be very cool to get an solution for that.
Cheers
Moritz Weichert