Hi everyone,
I actually have the TM4C1294XL and plugged on it the extansion http://www.ti.com/tool/TIDM-TM4C129SDRAMNVM I downloaded the example but i have a problem when i'm compiling it after the importation.
I have the following error on the 3 projects :
#1966 cannot open source file "inc/hw_ints.h": Permission denied
I don't find where is the mistake, i saw some poeple had this problem before and i tryed the fixes without result. Other projects are working well on the same workspace ... I think the problem is on the versions because the file "hw_ints.h" is from the "SW-EK-TM4C1294XL-2.1.1.71" and the example seems to be for the "2.1.0.12573" version. I'm working on CCS Version: 6.1.1.00022.
I tryed to find the 2.1.0.12573 version but i only find the current version : 2.1.2.111.
How can i fix this problem please ?
Regards,
John