Other Parts Discussed in Thread: TLV320AIC3104, BOOSTXL-AUDIO
I know it's coming, it was announced over a year ago. Does anyone know when this boosterpack is finally going to be released?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV320AIC3104, BOOSTXL-AUDIO
I know it's coming, it was announced over a year ago. Does anyone know when this boosterpack is finally going to be released?
For the TIVA Launchpads.
There is a boosterpack by CircuitCo coming based on
Dr. Donald Reay on his newly released book on the TIVA x123 for DSP applications references it -->>
"........Cathy Wicks at the TI University Program and Hieu Duong at CircuitCo for developing the audio booster pack....."
Dr. Reay did reply to my inquiry a while back stating he expected it to come out soon.
It's been a while though!!
Not all collaborations - Academia & Industrial - proceed as hoped and/or expected. (and rarely to schedule)
I'd ask, "Who most benefits from a timely release?"
Pushing (there - the "stake-holders") - rather than (here - humble users) - seems, "more fertile ground." (perhaps even (almost) holy ground.)
Amit Ashara said:SPI emulated I2S application note for TM4C12x devices
Uh-oh - poster had such high hopes. We now learn that (only) via "emulation" may the proper interface be, "teased out."
Usually - but not always - such, "Franken-chip" methods prove sub-optimal. Dedicated & specialized interfaces exist for good reason - cobbling together some attachment seems of little merit when multiple, proper, (other) devices exist - loaded w/the exact interface required...
Not (all) marriages are made in heaven - this one seems to have escaped that blessing.
For whatever reason I did not get an email update that there was a reply :(
I know the reviewers of this board liked it. Emulated SPI to I2S would be ok I think. The price point I believe is coming would also bring the TIVA x123 to a really nice standing with the competition.
But from the looks of it no one has heard of this board yet.
There is a very specific full board referenced on Dr. Reay (one of the leading Professors/reasearchers on Real Time DSP)...
See a very specific mention on his book:
onlinelibrary.wiley.com/.../summary
Inside the book he gives some more info. I have been in contact with him in the last year and he has worked with this board already producing materials/software for it which you can see on his download materials already. I at least know of a University interested on this board so at least some demand is there (perhaps not enough to push it faster, or at all).
The TIVA series are probably among the cheapest and still robust ARM boards out there. But for RTDSP they lack the codec, which this board would address. There is already a boosterpack with a codec in TI's listing but they charge way too much for it and so it will not take off (IMO) so there is no point in using it if it would only be a one-off to learn how to use it.
CircuitCo I believe is the manufacturer and as I stated before they were close 6 months ago. Perhaps they hit a priority bump or whatever. Maybe we'll never see this board....but if there is a place to ask, isn't it here?
Hi Thiago,
The BOOSTXL-AUDIO booster pack won't work (straightforwardly) with the TM4C123 Launchpad. It's designed for use with the MSP432. Frustratingly, and despite all being based on an ARM Cortex-M4 core, the TM4C123, TM4C129 and MSP432 each have different I2S (or I2S-equivalent) peripherals. Furthermore, I2S ((one) industry standard for audio data interface between microcontroller and codec device) is not covered by the launchpad/booster pack interface standard.
In any case, the BOOSTXL-AUDIO booster pack doesn't have the capabilities of a dedicated stereo audio codec. As far as I am aware, it is mono, the DAC provided is not a dedicated audio DAC, and the microphone input is routed to the 'instrumentation specification' ADC in the MSP432 without 'audio spec.' antialiasing.
I don't know why circuitco haven't manufactured the AIC3104-based audio booster pack that we developed.
As I've mentioned previously, if I were to recommend a hardware platform for use with my book, it would be the Cypress FM4 Pioneer board.
However, I'm hoping shortly to add to the companion website for the book a version of the software to work with the original prototype audio booster pack that I first built in 2013. Also, I hope to add the pcb artwork so that people will have the option of fabricating this themselves.
The design is based on the same codec (TI AIC23/Cirrus Logic WM8731) as used in the C6713 DSK and in the Cypress FM4 board. I've attached images of the first prototype board. This used an AIC23 codec and Lumberg jack sockets. I am just testing a slightly different version of the boosterpack that uses the less expensive Cirrus Logic WM8731 codec and more widely available Switchccraft jack sockets.
Donald