This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 Uart Bootloader SCI

Hi,

I am working on tms570 Uart Bootloader application note and its code. This code works very well. I want to use other SCI port to communicate, I figured out that if I change sciREG1 and sciREG2, sciPORT1 and sciPORT2 adresses each other, communication should work on other SCI port. RX port works well but TX port did not work. Why tx pin did not work

* This pointer is used by the SCI driver to access the sci module registers.
*/
#define sciREG1 ((sciBASE_t *)0xFFF7E500U)


/** @def sciPORT1
* @brief SCI1 GIO Port Register Pointer
*
* Pointer used by the GIO driver to access I/O PORT of SCI1
* (use the GIO drivers to access the port pins).
*/
#define sciPORT1 ((gioPORT_t *)0xFFF7E540U)


/** @def sciREG2
* @brief SCI2 Register Frame Pointer
*
* This pointer is used by the SCI driver to access the sci module registers.
*/
#define sciREG2 ((sciBASE_t *)0xFFF7E400U)


/** @def sciPORT2
* @brief SCI2 GIO Port Register Pointer
*
* Pointer used by the GIO driver to access I/O PORT of SCI2
* (use the GIO drivers to access the port pins).
*/
#define sciPORT2 ((gioPORT_t *)0xFFF7E440U)

How can i work with other sci port.

  • Hi,
    Are you in SCI mode or LIN mode? Can you make sure the SCIGCR1.6 bit is 0 so the LIN/SCI module is operating in SCI mode?

    I also want to know if you can toggle the TX pin in GIO mode. If you do the below, do you see the TX pin goes high?

    gioSetDirection(sciPORT2, 0x4); // set TX pin to output pin
    gioSetBit(sciPORT2, 0x4, 0x1); // set TX pin to high

    Make sure that you are in digital I/O mode for the above test with SCIPIO0=0x0. You can do the above test in the debugger too.
  • Hi,

     Not sure if you have resolved your problem? I'd like to know what device you have. Also in your post I'm not clear if you were changing from SCI1 to SCI2 or from SCI2 to SCI1.

     Normally, the SCI1 is mapped to 0xFFF7_E500 and the LIN/SCI2 is mapped to 0xFFF7_E400. You might have started your bootloader using the SCI/LIN (@0xFFF7_E400) and wanting to switch to SCI module (@ 0xFFF7_E500) to perform the same bootloading capablity. If this is a case, then I can see one problem. The issue is that the SCITX signal is multiplexed with the NHET1[13] signal. NHET1[13] is the default function brought to the device pin. If you want to bring out the SCITX functionality you will need to program the IOMM (PinMux Module) module. See the IOMM chapter in your device specific TRM.

  • Hi.

    Thanks to all for your replies,

    I have attached  document and source code of bootloader. i have tms570ls31. Charles you are right, Bootloader code using SCI-LIN port, and i want to change to SCI port. i looked at pinmux.

    void Gladiator_PINMUX_SCI2()
    {
    *(int *) 0xFFFFEB30 = 0x01010102;//P8 //SCITX
    *(int *) 0xFFFFEB2C = 0x01020101;//P7 //SCIRX
    }

    I could not see problem on pinmux. 

    void Gladiator_PINMUX_NHET2()
    {
    *(int *) 0xFFFFEB14 = 0x01010401;//p1 //NHET2[18]
    *(int *) 0xFFFFEB18 = 0x01020108;//p2 //NHET2[2],NHET2[0]
    *(int *) 0xFFFFEB1C = 0x01020101;//p3 //NHET2[4]
    *(int *) 0xFFFFEB20 = 0x10100102;//p4 //NHET2[10],NHET2[8],NHET2[6]
    *(int *) 0xFFFFEB24 = 0x01040101;//p5 //NHET2[12]
    *(int *) 0xFFFFEB28 = 0x01020108;//p6 //NHET2[16],NHET2[3]
    *(int *) 0xFFFFEB38 = 0x01040101;//p10 //NHET2[7]
    *(int *) 0xFFFFEB3C = 0x01010104;//p11 //NHET2[9]
    *(int *) 0xFFFFEB48 = 0x02010101;//p14 //NHET2[5]
    *(int *) 0xFFFFEB64 = 0x01010102;//p21 //NHET2[3]
    *(int *) 0xFFFFEB68 = 0x01040402;//p22 //NHET2[11],NHET2[13],NHET2[1]
    *(int *) 0xFFFFEB6C = 0x01010104;//p23 //NHET2[15]
    }

    SCI init is

    void sciInit(void)
    {
    /** @b intalise @b SCI1 */
    unsigned f;
    double vclk = SYS_CLK_FREQ * 1000000 / 2;

    /** - bring SCI out of reset */
    sciREG1->GCR0 = 1U;

    /** - Disable all interrupts */
    sciREG1->CLRINT = 0xFFFFFFFF;
    sciREG1->CLRINTLVL = 0xFFFFFFFF;

    /** - global control 1 */
    sciREG1->GCR1 = (1 << 25) /* enable transmit */
    | (1 << 24) /* enable receive */
    | (1 << 5) /* internal clock (device has no clock pin) */
    | (0 << 4) /* number of stop bits */
    | (0 << 3) /* even parity, otherwise odd */
    | (0 << 2) /* enable parity */
    | (1 << 1) /* asynchronous timing mode */
    | (0 << 0);

    /** - set baudrate */
    // sciREG1->BAUD = 42; /* 115.20K baudrate for 160MHz Vclk */
    // sciREG1->BAUD = 259; /* 19.2K baudrate for 160MHz Vclk */
    // sciREG1->BAUD = 155; /* 19.2K baudrate for 96MHz Vclk */

    f = sciREG1->GCR1 & 2 ? 16 : 1;
    sciREG1->BAUD = ((unsigned)((vclk /(f*UART_BAUDRATE) + 0.5)) - 1) & 0x00FFFFFF;


    /** - tranmision length */
    sciREG1->LENGTH = 7; /* length is 7+1 */

    /** - set SCI pins functional mode */
    sciREG1->FUN = (1 << 2) /* tx pin */
    | (1 << 1) /* rx pin */
    | (0); /* clk pin */

    /** - set SCI pins default output value */
    sciREG1->DOUT = (0 << 2) /* tx pin */
    | (0 << 1) /* rx pin */
    | (0); /* clk pin */

    /** - set SCI pins output direction */
    sciREG1->DIR = (0 << 2) /* tx pin */
    | (0 << 1) /* rx pin */
    | (0); /* clk pin */

    /** - set SCI pins open drain enable */
    sciREG1->ODR = (0 << 2) /* tx pin */
    | (0 << 1) /* rx pin */
    | (0); /* clk pin */

    /** - set SCI pins pullup/pulldown enable */
    sciREG1->PD = (1 << 2) /* tx pin */
    | (1 << 1) /* rx pin */
    | (0); /* clk pin */

    /** - set SCI pins pullup/pulldown select */
    sciREG1->PSL = (1 << 2) /* tx pin */
    | (1 << 1) /* rx pin */
    | (1); /* clk pin */

    /** - set interrupt level */
    sciREG1->SETINTLVL = (0 << 26) /* Framing error */
    | (0 << 25) /* Overrun error */
    | (0 << 24) /* Pariry error */
    | (0 << 9) /* Receive */
    | (0 << 8) /* Transmit */
    | (0 << 1) /* Wakeup */
    | (0); /* Break detect */

    /** - set interrupt enable */
    sciREG1->SETINT = (0 << 26) /* Framing error */
    | (0 << 25) /* Overrun error */
    | (0 << 24) /* Pariry error */
    | (0 << 9) /* Receive */
    | (0 << 1) /* Wakeup */
    | (0); /* Break detect */

    /** - inialise global transfer variables */
    g_sciTransfer[0].mode = 0 << 8;
    g_sciTransfer[0].length = 0;

    /** - Finaly start SCI1 */
    sciREG1->GCR1 |= 0x80;

    i could not see problem on sci init. function. When i change memory map of the SCI and SCI-LIN resgisters, code should work and i should communicate with SCI port. But i Should not communicate.

    i thought it would be a problem with baud rate.  VCLK1 is 80 mhz, its source is pll1 and both of them was  the required value . I do not understand problem.

    0550.spna193.zip1425.spna193.pdf

  • hi all,

    I have solved my problem. I forgot to unlock CPU write access.

       *(int *) 0xFFFFEA38  = 0x83E70B13; 
        *(int *) 0xFFFFEA3C  = 0x95A4F1E0;
     
        *(int *) 0xFFFFEB30 = 0x01010102;//P8  //SCITX
        *(int *) 0xFFFFEB2C = 0x01020101;//P7  //SCIRX
     
        *(int *) 0xFFFFEA38  = 0x00000000; 
        *(int *) 0xFFFFEA3C  = 0x00000000;

    Sorry for taking your time. Thanks all.

  • Hi,
    Glad your problem is resolved. Can you please close the thread by clicking the 'verify answer' button? Thanks.