Other Parts Discussed in Thread: HALCOGEN
In our company we bought 2 pieces of this development kit and in short time both have failed with the same failure. After some time using it, the LDO which generates the 3V3 rail is heating up and the rail goes down (TPS73733QDRBRQ1). This also causes the 1V2 rail to go down. It may be that the the rail is down because of the internal thermal/current protection of the device. The failure is not reversible, it doesn't dissapear by shutting down and letting cool down the board. It looks like there is some hardware design error causing the LDO to fail after some time, perhaps it is dimensioned for too small current...
The board is used in a normal way. It is powered with the adapter delivered with the board (part of the kit). Code is generated with HALCoGen for the correct board, so drivers for peripherals are (should be) configured correctly. No modifications to the boards have been made and the interfaces are used in a normal way (Ethernet and USB for programming).
Is this problem familiar to someone?