Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C123GXL
I am using Keil uVision4.74 in windows 8 platform for programming my Tiva boards ( EK-TM4C1294XL and EK-TM4C123GXL launchpad).
Some times my keil used to crash during debugging, then the only solution was to quit the keil and start debugging again.
after some time, after restarting keil, it failed to detect the board. then i disconnected and reconnected the board, now its not getting detected in PCs device manager itself. So unable to use LM flash tool also.
The power supply to the board is working ,with power LED ON indication. I could measure +5V & 3.3 V in the board when it is powered up.
What I should do , can anyone provide a solution to recover the boards?
Thanks in advance