Other Parts Discussed in Thread: LAUNCHXL2-570LC43
Hello,
I have LAUNCHXL2-570LC43. And I am trying to start developing with it.
I have installed Code Composer Studio V6.0.1.00040 and update packages "Hercules Emulation" to version 6.0.7 and TI Emulators to version 6.0.83.1
When I connect the board to my computer I can see two devices in the device administrator:
XDS110 Class Application/User UART (COM7) --> driver is successfully installed.
XDS110 Class Auxiliary Data Port (COM8) --> driver is NOT installed successfully.
When I try to open the serial port COM7 with Termite/Hyperterminal... there is an error while opening the Port.
I am using Windows XP (not sure whether this is relevant)
I am missing to install something?
Thanks for helping.
Francis.