Other Parts Discussed in Thread: TMS570LS3137
Hello,
I have seen that the new revision D of the TMS570LS3137 fixes two bugs related to the EMIF
- erratum DEVICE#B064: Incorrect Write to External Memory using Store-Multiple CPU instruction
- erratum DEVICE#B071: CPU write to peripheral or EMIF may be lost
In the revision C, the workaround for these bugs were (roughly) to prevent the compiler to use the STMxx instructions. Especially in the case of the DEVICE#B064, it is stated in the message that for Revision D, the workaround can be deleted in order to re-gain EMIF performance.
I cannot test the EMIF performance gain for now because I don't have the RevD samples yet, but I would be interested in having information from TI about what I can expect. Being able to evaluate the EMIF performances as soon as possible is really important for our project.
Best regards
PGC