Hi,
I've read the bootloader documentation which comes with the TivaWare distribution, but the ethernet section is a bit short and I'm missing some information. Is it (like for the serial protocol) possible to send the application address together/before with the firmware image when using ethernet to update an application? Or is the target address statically determined in bl_config?
Thanks!