Other Parts Discussed in Thread: EK-TM4C123GXL, TM4C123GH6PM
I am using the EK-TM4C123GXL LaunchPad, and the MKII Educational Booster Pack, When I run the code, it gives me the accelerometer data instead of the joystick data. I edited a code I have from earlier which would read the voltage on a potentiometer which is connected between 3.3v and ground. That code works, However when I try the same code, edited to target the Booster pack Joystick pins, J3.26, I get the accelerometer data. I even tried it with the horizontal axis of the joystick, but I get the same pin (J1.2). I am just mapping the launchpad pins which have different names, but they are in the same position. Am I just missing something? Are the pins of the TM4C which match the sockets of the booster pack not connected to an ADC?
- Using CCS 6.1.2.00015
- Using UART to display output
- Moving the joystick has no change in output
- Changing orientation of the booster pack changes the output from 0.99 to 2.33
- Original working code with potentiometer (original code)
- New code which gets me the accelerometer data is below is targeting the horizontal axis of the joystick (J1.2)
Here is the original code:
#include <stdint.h> // Variable definitions for the C99 standard.
#include <stdio.h> // Input and output facilities for the C99 standard.
#include <stdbool.h> // Boolean definitions for the C99 standard.
#include "inc/tm4c123gh6pm.h" // Definitions for the interrupt and register assignments.
#include "inc/hw_memmap.h" // Memory map definitions of the Tiva C Series device.
#include "inc/hw_types.h" // Definitions of common types and macros.
#include "inc/hw_gpio.h" // Defines and Macros for GPIO hardware.
#include "driverlib/sysctl.h" // Definitions and macros for System Control API of DriverLib.
#include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib.
#include "driverlib/gpio.h" // Definitions and macros for GPIO API of DriverLib.
#include "driverlib/timer.h" // Defines and macros for Timer API of DriverLib.
#include "driverlib/pin_map.h" //Mapping of peripherals to pins for all parts.
#include "driverlib/uart.h" // Definitions and macros for UART API of DriverLib.
#include "driverlib/adc.h" // Definitions for ADC API of DriverLib.
#include "driverlib/fpu.h" // Prototypes for the FPU manipulation routines.
#include "utils/uartstdio.h" // Prototypes for the UART console functions.
// Needs to add "utils/uartstdio.c" through a relative link.
#define TIMER0_FREQ 2 // Freqency in Hz, for blinking LED.
#define TIMER1_FREQ 1 // Frequency in Hz, for ADC.
#define UART0_BAUDRATE 115200 // UART baudrate in bps.
#define ADC0_SEQ_NUM 0 // ADC Sample Sequence Number
#define MAX_ADC_SAMP_VAL 0x0FFF // max value for 12-bit ADC
#define RED_LED GPIO_PIN_1
#define BLUE_LED GPIO_PIN_2
#define GREEN_LED GPIO_PIN_3
#define DISP_TEXT_LINE_NUM 4
#define DISP_DATA_STR_LEN 20
// function prototypes
void init_LEDs(void);
void init_GPIO(void);
void init_timer(void);
void init_UART(void);
void init_ADC(void);
void Timer0_ISR(void);
void Timer1_ISR(void);
extern void UARTStdioIntHandler(void);
// global variables
uint32_t sys_clock;
uint8_t cur_LED = RED_LED;
const char *disp_text[DISP_TEXT_LINE_NUM] = {
"\n",
"UART and LED Demo\n",
"H: help, R: red, G: green, B: blue, S: Sample Data.\n",
"> " };
uint32_t sig_data=0, sig_data_d;
float sig_data_f;
char disp_data_str[DISP_DATA_STR_LEN];
int main(void)
{
uint32_t i;
unsigned char user_cmd;
// Configure system clock at 40 MHz.
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
sys_clock = SysCtlClockGet();
// Enable the floating-point unit (FPU).
FPUEnable();
// Configure FPU to perform lazy stacking of the floating-point state.
FPULazyStackingEnable();
init_LEDs();
init_GPIO();
init_ADC();
init_UART();
init_timer();
// Enable the processor to respond to interrupts.
IntMasterEnable();
// Start the timer by enabling operation of the timer module.
TimerEnable(TIMER0_BASE, TIMER_A);
TimerEnable(TIMER1_BASE, TIMER_A);
// Initial display on terminal.
for(i=0; i<DISP_TEXT_LINE_NUM; i++)
UARTprintf(disp_text[i]);
while(1) {
// Read user inputs from UART if available.
if(UARTRxBytesAvail())
user_cmd = UARTgetc();
else
user_cmd = 0;
switch(user_cmd){
case '\r':
case ' ':
case 'H':
case 'h':
for(i=0; i<DISP_TEXT_LINE_NUM; i++)
UARTprintf(disp_text[i]);
break;
case 'R':
case 'r':
cur_LED = RED_LED;
UARTprintf("\n> ");
break;
case 'B':
case 'b':
cur_LED = BLUE_LED;
UARTprintf("\n> ");
break;
case 'G':
case 'g':
cur_LED = GREEN_LED;
UARTprintf("\n> ");
break;
case 'S':
case 's':
ADCProcessorTrigger(ADC0_BASE, ADC0_SEQ_NUM);
while(!ADCIntStatus(ADC0_BASE, ADC0_SEQ_NUM, false)) {
}
ADCIntClear(ADC0_BASE, ADC0_SEQ_NUM);
ADCSequenceDataGet(ADC0_BASE, ADC0_SEQ_NUM, &sig_data);
sig_data_f = 3.3*sig_data/MAX_ADC_SAMP_VAL;
if(GPIOPinRead(GPIO_PORTE_BASE, GPIO_PIN_4))
sig_data_d = 1;
else
sig_data_d = 0;
// Print data to UART0
snprintf(disp_data_str, DISP_DATA_STR_LEN, "v=%.2f, d=%d", sig_data_f, sig_data_d);
UARTprintf("\n%s\n> ", disp_data_str);
break;
}
}
}
void init_LEDs(void)
{
// Enable and configure LED peripheral.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // Enable GPIO Port F.
// Three onboard LEDs, R:PF1, B:PF2, G:PF3.
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
}
void init_timer(void)
{
// Enable and configure timer peripheral.
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
// Configure Timer0 as a 32-bit timer in periodic mode.
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
// Initialize timer load register.
TimerLoadSet(TIMER0_BASE, TIMER_A, sys_clock/TIMER0_FREQ -1);
// Configure Timer1 as a 32-bit timer in periodic mode.
TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
// Initialize timer load register.
TimerLoadSet(TIMER1_BASE, TIMER_A, sys_clock/TIMER1_FREQ -1);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_TIMER0A, Timer0_ISR);
// The specified interrupt is enabled in the interrupt controller.
IntEnable(INT_TIMER0A);
// Enable the indicated timer interrupt source.
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_TIMER1A, Timer1_ISR);
// The specified interrupt is enabled in the interrupt controller.
IntEnable(INT_TIMER1A);
// Enable the indicated timer interrupt source.
TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
}
void init_UART(void)
{
// Enable and configure UART0 for debugging printouts.
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_UART0, UARTStdioIntHandler);
UARTStdioConfig(0, UART0_BAUDRATE, sys_clock);
}
void init_ADC(void)
{
// Enable and configure ADC0. Sample from PD0/AIN7/BY
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_0);
ADCSequenceConfigure(ADC0_BASE, ADC0_SEQ_NUM, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, ADC0_SEQ_NUM, 0, ADC_CTL_IE|ADC_CTL_CH7|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, ADC0_SEQ_NUM);
}
void init_GPIO(void)
{
// Enable and configure PE4 as digital input
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeGPIOInput(GPIO_PORTE_BASE, GPIO_PIN_4);
}
// Timer0 interrupt service routine
void Timer0_ISR(void)
{
// Clear the timer interrupt.
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
// Blink LED. Read the current state of GPIO pins and write back the opposite state.
if(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3)) {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0);
}
else {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, cur_LED);
}
}
void Timer1_ISR(void)
{
// Clear the timer interrupt.
TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ADCProcessorTrigger(ADC0_BASE, ADC0_SEQ_NUM);
while(!ADCIntStatus(ADC0_BASE, ADC0_SEQ_NUM, false)) {
}
ADCIntClear(ADC0_BASE, ADC0_SEQ_NUM);
ADCSequenceDataGet(ADC0_BASE, ADC0_SEQ_NUM, &sig_data);
sig_data_f = 3.3*sig_data/MAX_ADC_SAMP_VAL;
if(GPIOPinRead(GPIO_PORTE_BASE, GPIO_PIN_4))
sig_data_d = 1;
else
sig_data_d = 0;
// Print data to UART0
snprintf(disp_data_str, DISP_DATA_STR_LEN, "v=%.2f, d=%d", sig_data_f, sig_data_d);
UARTprintf("\n%s\n> ", disp_data_str);
}
New non working code:
#include <stdint.h> // Variable definitions for the C99 standard.
#include <stdio.h> // Input and output facilities for the C99 standard.
#include <stdbool.h> // Boolean definitions for the C99 standard.
#include "inc/tm4c123gh6pm.h" // Definitions for the interrupt and register assignments.
#include "inc/hw_memmap.h" // Memory map definitions of the Tiva C Series device.
#include "inc/hw_types.h" // Definitions of common types and macros.
#include "inc/hw_gpio.h" // Defines and Macros for GPIO hardware.
#include "driverlib/sysctl.h" // Definitions and macros for System Control API of DriverLib.
#include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib.
#include "driverlib/gpio.h" // Definitions and macros for GPIO API of DriverLib.
#include "driverlib/timer.h" // Defines and macros for Timer API of DriverLib.
#include "driverlib/pin_map.h" //Mapping of peripherals to pins for all parts.
#include "driverlib/uart.h" // Definitions and macros for UART API of DriverLib.
#include "driverlib/adc.h" // Definitions for ADC API of DriverLib.
#include "driverlib/fpu.h" // Prototypes for the FPU manipulation routines.
#include "utils/uartstdio.h" // Prototypes for the UART console functions.
// Needs to add "utils/uartstdio.c" through a relative link.
#define TIMER0_FREQ 2 // Freqency in Hz, for blinking LED.
#define TIMER1_FREQ 1 // Frequency in Hz, for ADC.
#define UART0_BAUDRATE 115200 // UART baudrate in bps.
#define ADC0_SEQ_NUM 0 // ADC Sample Sequence Number
#define MAX_ADC_SAMP_VAL 0x0FFF // max value for 12-bit ADC
#define RED_LED GPIO_PIN_1
#define BLUE_LED GPIO_PIN_2
#define GREEN_LED GPIO_PIN_3
#define DISP_TEXT_LINE_NUM 4
#define DISP_DATA_STR_LEN 20
// function prototypes
void init_LEDs(void);
void init_GPIO(void);
void init_timer(void);
void init_UART(void);
void init_ADC(void);
void Timer0_ISR(void);
void Timer1_ISR(void);
extern void UARTStdioIntHandler(void);
// global variables
uint32_t sys_clock;
uint8_t cur_LED = RED_LED;
const char *disp_text[DISP_TEXT_LINE_NUM] = {
"\n",
"UART and LED Demo\n",
"H: help, R: red, G: green, B: blue, S: Sample Data.\n",
"> " };
uint32_t sig_data=0, sig_data_d;
float sig_data_f;
char disp_data_str[DISP_DATA_STR_LEN];
int main(void)
{
uint32_t i;
unsigned char user_cmd;
// Configure system clock at 40 MHz.
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
sys_clock = SysCtlClockGet();
// Enable the floating-point unit (FPU).
FPUEnable();
// Configure FPU to perform lazy stacking of the floating-point state.
FPULazyStackingEnable();
init_LEDs();
init_GPIO();
init_ADC();
init_UART();
init_timer();
// Enable the processor to respond to interrupts.
IntMasterEnable();
// Start the timer by enabling operation of the timer module.
TimerEnable(TIMER0_BASE, TIMER_A);
TimerEnable(TIMER1_BASE, TIMER_A);
// Initial display on terminal.
for(i=0; i<DISP_TEXT_LINE_NUM; i++)
UARTprintf(disp_text[i]);
while(1) {
// Read user inputs from UART if available.
if(UARTRxBytesAvail())
user_cmd = UARTgetc();
else
user_cmd = 0;
switch(user_cmd){
case '\r':
case ' ':
case 'H':
case 'h':
for(i=0; i<DISP_TEXT_LINE_NUM; i++)
UARTprintf(disp_text[i]);
break;
case 'R':
case 'r':
cur_LED = RED_LED;
UARTprintf("\n> ");
break;
case 'B':
case 'b':
cur_LED = BLUE_LED;
UARTprintf("\n> ");
break;
case 'G':
case 'g':
cur_LED = GREEN_LED;
UARTprintf("\n> ");
break;
case 'S':
case 's':
ADCProcessorTrigger(ADC0_BASE, ADC0_SEQ_NUM);
while(!ADCIntStatus(ADC0_BASE, ADC0_SEQ_NUM, false)) {
}
ADCIntClear(ADC0_BASE, ADC0_SEQ_NUM);
ADCSequenceDataGet(ADC0_BASE, ADC0_SEQ_NUM, &sig_data);
sig_data_f = 3.3*sig_data/MAX_ADC_SAMP_VAL;
if(GPIOPinRead(GPIO_PORTB_BASE, GPIO_PIN_5))
sig_data_d = 1;
else
sig_data_d = 0;
// Print data to UART0
snprintf(disp_data_str, DISP_DATA_STR_LEN, "v=%.2f, d=%d", sig_data_f, sig_data_d);
UARTprintf("\n%s\n> ", disp_data_str);
break;
}
}
}
void init_LEDs(void)
{
// Enable and configure LED peripheral.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // Enable GPIO Port F.
// Three onboard LEDs, R:PF1, B:PF2, G:PF3.
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
}
void init_timer(void)
{
// Enable and configure timer peripheral.
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
// Configure Timer0 as a 32-bit timer in periodic mode.
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
// Initialize timer load register.
TimerLoadSet(TIMER0_BASE, TIMER_A, sys_clock/TIMER0_FREQ -1);
// Configure Timer1 as a 32-bit timer in periodic mode.
TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
// Initialize timer load register.
TimerLoadSet(TIMER1_BASE, TIMER_A, sys_clock/TIMER1_FREQ -1);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_TIMER0A, Timer0_ISR);
// The specified interrupt is enabled in the interrupt controller.
IntEnable(INT_TIMER0A);
// Enable the indicated timer interrupt source.
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_TIMER1A, Timer1_ISR);
// The specified interrupt is enabled in the interrupt controller.
IntEnable(INT_TIMER1A);
// Enable the indicated timer interrupt source.
TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
}
void init_UART(void)
{
// Enable and configure UART0 for debugging printouts.
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// Registers a function to be called when the interrupt occurs.
IntRegister(INT_UART0, UARTStdioIntHandler);
UARTStdioConfig(0, UART0_BAUDRATE, sys_clock);
}
void init_ADC(void)
{
// Enable and configure ADC0. Sample from PD0/AIN7/BY
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
GPIOPinTypeADC(GPIO_PORTB_BASE, GPIO_PIN_5);
ADCSequenceConfigure(ADC0_BASE, ADC0_SEQ_NUM, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, ADC0_SEQ_NUM, 0, ADC_CTL_IE|ADC_CTL_CH7|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, ADC0_SEQ_NUM);
}
void init_GPIO(void)
{
// Enable and configure PE4 as digital input
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_5);
}
// Timer0 interrupt service routine
void Timer0_ISR(void)
{
// Clear the timer interrupt.
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
// Blink LED. Read the current state of GPIO pins and write back the opposite state.
if(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3)) {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0);
}
else {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, cur_LED);
}
}
void Timer1_ISR(void)
{
// Clear the timer interrupt.
TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ADCProcessorTrigger(ADC0_BASE, ADC0_SEQ_NUM);
while(!ADCIntStatus(ADC0_BASE, ADC0_SEQ_NUM, false)) {
}
ADCIntClear(ADC0_BASE, ADC0_SEQ_NUM);
ADCSequenceDataGet(ADC0_BASE, ADC0_SEQ_NUM, &sig_data);
sig_data_f =3.3*sig_data/MAX_ADC_SAMP_VAL;
if(GPIOPinRead(GPIO_PORTB_BASE, GPIO_PIN_5))
sig_data_d = 1;
else
sig_data_d = 0;
// Print data to UART0
snprintf(disp_data_str, DISP_DATA_STR_LEN, "v=%.2f, d=%d", sig_data_f, sig_data_d);
UARTprintf("\n%s\n> ", disp_data_str);
}