Other Parts Discussed in Thread: HALCOGEN
Hi!
Iam training with TMS570 and right now my goal is to learn how to set up and use ADC1group1 conversion ready IRQ.
In HALCOGEN i have set up following:
Enable ADC1 driver,
set cycle time,
enable pin 9 (ambient light sensor on HDK)
VIM channel 0-31 i have enabled ADC1 Group 1 IRQ
My main looks like this:
- in endless loop i start conversion and then there is hudge dummy wait time (decrementing i) where i only test if flag == 1;. flag is my global variable that i set to 1 in void adc1Group1Interrupt(void) that is part of HL_adc.h library. When debugging, i have found out that program never go into that handler ... why?
Am I missing something? I have allowed IRQ globally in init part of main. Do i have to allow that specific IRQ "locally" ?
Thanks a lot for your answer
regards
Jan Slavotínek
Honeywell aerospace technical support
void main(void)
{
/* USER CODE BEGIN (3) */
sciInit(); /* initialize sci/sci-lin */
/* even parity , 2 stop bits */
adcInit();
_enable_IRQ_interrupt_();
/*_enable_interrupt_();*/
while(true)
{
adcStartConversion(adcREG1, adcGROUP1);
/*
while((adcIsConversionComplete(adcREG1,adcGROUP1))==0);
adcGetData(adcREG1, adcGROUP1,&adc_data);
ConvertSendValue(adc_data.value);
*/
i = 10000000;
while(i--)
{
switch(flag)
{
case 1:
flag = 0;
adcGetData(adcREG1, adcGROUP1,&adc_data);
ConvertSendValue(adc_data.value);
break;
default:
break;
}
}
}
/* USER CODE END */
}