Other Parts Discussed in Thread: RM41L232, RM44L520
Hi, I have noticed in the data sheets for various Hercules controllers that some controllers have very small differences between these two numbers and some have big differences.
For example,
RM41L232's operational current is 135 typical and 145 maximum.
RM44L520 (120 MHz)'s operational current is 120 typical and 260 maximum, a huge difference.
I am asking this because I need a system with more than 32 kB of RAM (preferably 64k or 128k), but if I have to account for the maximum power ratings, my power budget will go through the roof.
So why are these numbers so different (max vs typical)? And which numbers should I take into account when specifying the power requirements?