This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Microframe interrupt?

In TM4C1294/CCS/TivaWare-2.1.0.12573

I think USB_INTCTRL_SOF is the interrupt flag for USB Start-of-frame (1ms interval).

Any similar flag for the microframe (1/8 ms, used by USB 2.0 highspeed mode)?

I tried the USB sample project on different USB ports on different PCs and I only see the 1ms SOF

Thanks for pointers