Other Parts Discussed in Thread: CC2650
Using a CC2650 Launchpad with TM4C128 processor. Plan to run Bluetooth LE PHY testing with a Rohde&Schwarz CMW270 tester using USB for HCI interface.
The CMW270 are running Windows Embedded Standard (7) , SP1. When installing the XDS110 driver the following message is displayed
"Windows found driver software for your device but encountered an error while attempting to install it.
XDS110 Class Application/User UART
The system cannot find the file specified"
The driver version is 11/25/2014,1.6.0.0
Appreciate any help.
Regards,
Sven