Dear Ti,
I'm having trouble with J-Link after updaring to the latest CCS 6.1.2. I have followed the steps at "www.segger.com/ti-code-composer-studio.html" however I'm afraid that
"In the current version of CCS (V6.1.x), only some devices can be used with J-Link due to CCS internal incompatibilities which need to be corrected by TI, as they are out of the control of SEGGER. SEGGER can currently not provide a list of device which can already be used and which probably need some patching of certain files inside CCS"
applies to this case. I'm trying to debug TMS570LS3137 device. I'm getting the following error when trying to debug
Error connecting to the target:
ERROR in JLINKARM_Open: Can not connect to J-Link via USB.
I get the same message when I go to the SEGGER folder on my HDD and run the JLink.exe. Please note that this used to be working with an older JLink from SEGGER. If there's nothing I can do could you at least suggest to me an older combination of CCS (before v6) and Segger JLink (from www.segger.com/j-link-older-versions.html)
Thank you in advance,
Martin