Other Parts Discussed in Thread: EK-TM4C123GXL
I am trying to use UART studio to see the output of the of my sensor, but I kept getting this error
"C:/ti/TivaWare_C_Series-2.1.2.111/driverlib/gpio.h", line 141: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-2.1.2.111/driverlib/gpio.h", line 141: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-2.1.2.111/driverlib/gpio.h", line 142: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-2.1.2.111/driverlib/gpio.h", line 143: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-2.1.2.111/driverlib/gpio.h", line 143: error #20: identifier "uint32_t" is undefined
Description Resource Path Location Type
#20 identifier "bool" is undefined .ccsproject /ADC_Temp line 153, external location: C:\ti\TivaWare_C_Series-2.1.2.111\driverlib\gpio.h C/C++ Problem
#20 identifier "int32_t" is undefined .ccsproject /ADC_Temp line 157, external location: C:\ti\TivaWare_C_Series-2.1.2.111\driverlib\gpio.h C/C++ Problem
#20 identifier "uint32_t" is undefined .ccsproject /ADC_Temp line 141, external location: C:\ti\TivaWare_C_Series-2.1.2.111\driverlib\gpio.h C/C++ Problem
#20 identifier "uint32_t" is undefined .ccsproject /ADC_Temp line 142, external location: C:\ti\TivaWare_C_Series-2.1.2.111\driverlib\gpio.h C/C++ Problem
#20 identifier "uint32_t" is undefined .ccsproject /ADC_Temp line 143, external location: C:\ti\TivaWare_C_Series-2.1.2.111\driverlib\gpio.h C/C++ Problem