Other Parts Discussed in Thread: HALCOGEN
Hello
I am trying to implement a gio interrupt on my TMS57004 board. i want a rising edge trigger which when recorded should make the onboard LED GIOA2 glow.
this is my code-
#include"gio.h"
#include "sys_common.h"
void main(void)
{
/* USER CODE BEGIN (3) */
gioInit();
_enable_IRQ();
gioEnableNotification(gioPORTA,1);
}
/* USER CODE BEGIN (4) */
void gioNotification(gioPORT_t *port, uint32 bit)
{
gioSetBit(port,bit,1);
}
/* USER CODE END */
all the necessary settings have been made in the halcogen file.
However it is not working. when I try to do the same thing via polling it works fine.
Could someone please tell me where i am going wrong.
Thanks