Other Parts Discussed in Thread: SN754410
Hi,
I was working on project to control the the speed of motor using PWM . I use SN754410 bridge for my motor driver. I set up PWM for my motor in my code. But the code that I write does not run my motor. Below here is my code:
#define PWM_FREQUENCY 55
int main(void)
{
volatile uint32_t ui32Load;
volatile uint32_t ui32PWMClock;
volatile uint8_t ui8Adjust=100;
ROM_SysCtlClockSet( SYSCTL_SYSDIV_16 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
ROM_GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_4|GPIO_PIN_5);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
ROM_GPIOPinConfigure(GPIO_PB4_M0PWM2);
ROM_GPIOPinConfigure(GPIO_PB5_M0PWM3);
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
ui32PWMClock = SysCtlClockGet() / 64;
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_UP_DOWN);
PWMGenConfigure(PWM0_BASE, PWM_GEN_3, PWM_GEN_MODE_UP_DOWN);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, ui32Load);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_3, ui32Load);
ROM_PWMOutputState(PWM0_BASE, PWM_OUT_2_BIT|PWM_OUT_3_BIT, true);
ROM_PWMGenEnable(PWM0_BASE, PWM_GEN_1);
ROM_PWMGenEnable(PWM0_BASE, PWM_GEN_3);
while(1)
{
if(ROM_GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_4)==0x00)
{
ROM_PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, ui32Load / 1000);
ROM_PWMPulseWidthSet(PWM0_BASE, PWM_OUT_3, 0);
}
}
}
Thanks,
Fer