Hi Support,
What will be the impedance of IO pin while the MCU is OFF condition.
Facing some weird behavior in one of the IO pin.
PQ4 was used as output pin and connected to a voltage divider resistor network .
This resistor some time may have a voltage of 3.00V (from charger input voltage) even when the MCU is OFF.
The issue is voltage across the resistor is 0.6V where as expected voltage is 3.00V( Input voltage was 33V and resistor divider circuit made using 100K and 10K combination) .
Expected Voltage @ 10K resistor is 3V but getting less voltage because that resistor connected to MCU Pin PQ4.
When 33V applied there Is no 3.3V so MCU is not up.
Thanks.