This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Run and load Hercules TMS570LS3137 program in RAM instead of Flash

Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN

I'm working on a custom designed board based on TMS570LS3137 using the emulator XDS100v2 using Code Composer Studio 5.4.

After clicking on debug, the code gets sucessfully programmed into the flash. However, I need to run the code in the RAM instead of Flash to avoid exhausting the read/write cycles of the Flash.
I need to know the files and settings needed to be modified and the details to be taken care of while doing that, such as to avoid conflicts at startup etc.
We have followed the thread https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/210010 but we're facing problems such as mentioned below:

As per the thread mentioned , we have changed the GEL file OnTargetConnect() function to include the swap_mem(RAM) function and changed  sys_core.asm to have location of Stack pointers from "0x0800 0000" to "0x0000 0000". The program goes into debug session without giving any errors. However, the program goes into infinite loop in sys_startup.c file (line no. 267 in the file attached)

/** @file sys_startup.c 
*   @brief Startup Source File
*   @date 28.Aug.2015
*   @version 04.05.01
*
*   This file contains:
*   - Include Files
*   - Type Definitions
*   - External Functions
*   - VIM RAM Setup
*   - Startup Routine
*   .
*   which are relevant for the Startup.
*/

/* 
* Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com 
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */


/* Include Files */

#include "sys_common.h"
#include "system.h"
#include "sys_vim.h"
#include "sys_core.h"
#include "sys_selftest.h"
#include "esm.h"
#include "mibspi.h"

/* USER CODE BEGIN (1) */
/* USER CODE END */


/* USER CODE BEGIN (2) */
/* USER CODE END */


/* External Functions */
/*SAFETYMCUSW 218 S MR:20.2 <APPROVED> "Functions from library" */
extern void __TI_auto_init(void);
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(main should be declared by the user)" */
extern void main(void);
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(Extern declaration present in the library)" */
extern void exit(int _status);


/* USER CODE BEGIN (3) */
/* USER CODE END */

/* Startup Routine */
void _c_int00(void);
/* USER CODE BEGIN (4) */
/* USER CODE END */

#pragma CODE_STATE(_c_int00, 32)
#pragma INTERRUPT(_c_int00, RESET)
#pragma WEAK(_c_int00)

/* SourceId : STARTUP_SourceId_001 */
/* DesignId : STARTUP_DesignId_001 */
/* Requirements : HL_SR508 */
void _c_int00(void)
{
    
/* USER CODE BEGIN (5) */
/* USER CODE END */

    /* Initialize Core Registers to avoid CCM Error */
    _coreInitRegisters_();

/* USER CODE BEGIN (6) */
/* USER CODE END */

    /* Initialize Stack Pointers */
    _coreInitStackPointer_();

/* USER CODE BEGIN (7) */
/* USER CODE END */

    /* Work Around for Errata DEVICE#140: ( Only on Rev A silicon) 
     *
     * Errata Description:
     *            The Core Compare Module(CCM-R4) may cause nERROR to be asserted after a cold power-on
     * Workaround:
     *            Clear ESM Group2 Channel 2 error in ESMSR2 and Compare error in CCMSR register */
    if (DEVICE_ID_REV == 0x802AAD05U)
    {
        _esmCcmErrorsClear_();
    }
    
/* USER CODE BEGIN (8) */
/* USER CODE END */

    /* Enable CPU Event Export */
    /* This allows the CPU to signal any single-bit or double-bit errors detected
     * by its ECC logic for accesses to program flash or data RAM.
     */
    _coreEnableEventBusExport_();
/* USER CODE BEGIN (9) */
/* USER CODE END */

    /* Enable response to ECC errors indicated by CPU for accesses to flash */
    flashWREG->FEDACCTRL1 = 0x000A060AU;

/* USER CODE BEGIN (10) */
/* USER CODE END */

    /* Enable CPU ECC checking for ATCM (flash accesses) */
    _coreEnableFlashEcc_();
	

/* USER CODE BEGIN (11) */
/* USER CODE END */

        /* Workaround for Errata CORTEXR4 66 */
        _errata_CORTEXR4_66_();
    
        /* Workaround for Errata CORTEXR4 57 */ 
        _errata_CORTEXR4_57_();

    /* Reset handler: the following instructions read from the system exception status register
     * to identify the cause of the CPU reset.
     */

    /* check for power-on reset condition */
    /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
    if ((SYS_EXCEPTION & POWERON_RESET) != 0U)
    {
/* USER CODE BEGIN (12) */
/* USER CODE END */
        
        /* clear all reset status flags */
        SYS_EXCEPTION = 0xFFFFU;

/* USER CODE BEGIN (13) */
/* USER CODE END */
/* USER CODE BEGIN (14) */
/* USER CODE END */
/* USER CODE BEGIN (15) */
/* USER CODE END */
      /* continue with normal start-up sequence */
    }
    /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
    else if ((SYS_EXCEPTION & OSC_FAILURE_RESET) != 0U)
    {
        /* Reset caused due to oscillator failure.
        Add user code here to handle oscillator failure */

/* USER CODE BEGIN (16) */
/* USER CODE END */
    }
    /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
    else if ((SYS_EXCEPTION & WATCHDOG_RESET) !=0U)
    {
        /* Reset caused due 
         *  1) windowed watchdog violation - Add user code here to handle watchdog violation.
         *  2) ICEPICK Reset - After loading code via CCS / System Reset through CCS
         */
        /* Check the WatchDog Status register */
        if(WATCHDOG_STATUS != 0U)
        {
            /* Add user code here to handle watchdog violation. */ 
/* USER CODE BEGIN (17) */
/* USER CODE END */

            /* Clear the Watchdog reset flag in Exception Status register */ 
            SYS_EXCEPTION = WATCHDOG_RESET;
        
/* USER CODE BEGIN (18) */
/* USER CODE END */
        }
        else
        {
            /* Clear the ICEPICK reset flag in Exception Status register */ 
            SYS_EXCEPTION = ICEPICK_RESET;
/* USER CODE BEGIN (19) */
/* USER CODE END */
        }
    }
    /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
    else if ((SYS_EXCEPTION & CPU_RESET) !=0U)
    {
        /* Reset caused due to CPU reset.
        CPU reset can be caused by CPU self-test completion, or
        by toggling the "CPU RESET" bit of the CPU Reset Control Register. */

/* USER CODE BEGIN (20) */
/* USER CODE END */

        /* clear all reset status flags */
        SYS_EXCEPTION = CPU_RESET;

/* USER CODE BEGIN (21) */
/* USER CODE END */

    }
    /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
    else if ((SYS_EXCEPTION & SW_RESET) != 0U)
    {
        /* Reset caused due to software reset.
        Add user code to handle software reset. */

/* USER CODE BEGIN (22) */
/* USER CODE END */
    }
    else
    {
        /* Reset caused by nRST being driven low externally.
        Add user code to handle external reset. */

/* USER CODE BEGIN (23) */
/* USER CODE END */
    }

    /* Check if there were ESM group3 errors during power-up.
     * These could occur during eFuse auto-load or during reads from flash OTP
     * during power-up. Device operation is not reliable and not recommended
     * in this case.
     * An ESM group3 error only drives the nERROR pin low. An external circuit
     * that monitors the nERROR pin must take the appropriate action to ensure that
     * the system is placed in a safe state, as determined by the application.
     */

    if ((esmREG->SR1[2]) != 0U)
    {
/* USER CODE BEGIN (24) */
/* USER CODE END */
    /*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
    /*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
        for(;;)
        { 
        }/* Wait */                 
/* USER CODE BEGIN (25) */
/* USER CODE END */
    }

/* USER CODE BEGIN (26) */
/* USER CODE END */

    /* Initialize System - Clock, Flash settings with Efuse self check */
            systemInit();
    
    /* Workaround for Errata PBIST#4 */
    errata_PBIST_4();
	
    /* Run a diagnostic check on the memory self-test controller.
     * This function chooses a RAM test algorithm and runs it on an on-chip ROM.
     * The memory self-test is expected to fail. The function ensures that the PBIST controller
     * is capable of detecting and indicating a memory self-test failure.
     */
    pbistSelfCheck();	
	
	/* Run PBIST on STC ROM */
    pbistRun((uint32)STC_ROM_PBIST_RAM_GROUP,
             ((uint32)PBIST_TripleReadSlow | (uint32)PBIST_TripleReadFast));
    
    /* Wait for PBIST for STC ROM to be completed */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while(pbistIsTestCompleted() != TRUE)
    { 
    }/* Wait */ 
    
    /* Check if PBIST on STC ROM passed the self-test */
    if( pbistIsTestPassed() != TRUE)
    {
        /* PBIST and STC ROM failed the self-test.
         * Need custom handler to check the memory failure
         * and to take the appropriate next step.
         */
         
        pbistFail();

    }   
	
    /* Disable PBIST clocks and disable memory self-test mode */
    pbistStop();

	/* Run PBIST on PBIST ROM */
    pbistRun((uint32)PBIST_ROM_PBIST_RAM_GROUP,
             ((uint32)PBIST_TripleReadSlow | (uint32)PBIST_TripleReadFast));
    
    /* Wait for PBIST for PBIST ROM to be completed */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while(pbistIsTestCompleted() != TRUE)
    { 
    }/* Wait */ 
    
    /* Check if PBIST ROM passed the self-test */
    if( pbistIsTestPassed() != TRUE)
    {
        /* PBIST and STC ROM failed the self-test.
         * Need custom handler to check the memory failure
         * and to take the appropriate next step.
         */
         
        pbistFail();

    } 
	
    /* Disable PBIST clocks and disable memory self-test mode */
    pbistStop();	
/* USER CODE BEGIN (29) */
/* USER CODE END */

/* USER CODE BEGIN (31) */
/* USER CODE END */

    /* Disable RAM ECC before doing PBIST for Main RAM */
    _coreDisableRamEcc_();
    
    /* Run PBIST on CPU RAM.
     * The PBIST controller needs to be configured separately for single-port and dual-port SRAMs.
     * The CPU RAM is a single-port memory. The actual "RAM Group" for all on-chip SRAMs is defined in the
     * device datasheet.
     */
    pbistRun(0x08300020U, /* ESRAM Single Port PBIST */
             (uint32)PBIST_March13N_SP);

/* USER CODE BEGIN (32) */
/* USER CODE END */

    /* Wait for PBIST for CPU RAM to be completed */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while(pbistIsTestCompleted() != TRUE)
    { 
    }/* Wait */                 
    

/* USER CODE BEGIN (33) */
/* USER CODE END */
    
    /* Check if CPU RAM passed the self-test */
    if( pbistIsTestPassed() != TRUE)
    {
        /* CPU RAM failed the self-test.
         * Need custom handler to check the memory failure
         * and to take the appropriate next step.
         */
/* USER CODE BEGIN (34) */
/* USER CODE END */
         
        pbistFail();
        
/* USER CODE BEGIN (35) */
/* USER CODE END */
    }

/* USER CODE BEGIN (36) */
/* USER CODE END */

    /* Disable PBIST clocks and disable memory self-test mode */
    pbistStop();

    
/* USER CODE BEGIN (37) */
/* USER CODE END */


    /* Initialize CPU RAM.
     * This function uses the system module's hardware for auto-initialization of memories and their
     * associated protection schemes. The CPU RAM is initialized by setting bit 0 of the MSIENA register.
     * Hence the value 0x1 passed to the function.
     * This function will initialize the entire CPU RAM and the corresponding ECC locations.
     */
    memoryInit(0x1U);

/* USER CODE BEGIN (38) */
/* USER CODE END */
    
    /* Enable ECC checking for TCRAM accesses.
     * This function enables the CPU's ECC logic for accesses to B0TCM and B1TCM.
     */
    _coreEnableRamEcc_();

/* USER CODE BEGIN (39) */
/* USER CODE END */

    /* Start PBIST on all dual-port memories */
    /* NOTE : Please Refer DEVICE DATASHEET for the list of Supported Dual port Memories.
       PBIST test performed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
     */
    pbistRun(  (uint32)0x00000000U    /* EMAC RAM */
             | (uint32)0x00000000U    /* USB RAM */  
             | (uint32)0x00000800U    /* DMA RAM */
             | (uint32)0x00000200U    /* VIM RAM */
             | (uint32)0x00000000U    /* MIBSPI1 RAM */
             | (uint32)0x00000000U    /* MIBSPI3 RAM */
             | (uint32)0x00000000U    /* MIBSPI5 RAM */
             | (uint32)0x00000000U    /* CAN1 RAM */
             | (uint32)0x00000000U    /* CAN2 RAM */
             | (uint32)0x00000000U    /* CAN3 RAM */
             | (uint32)0x00000000U    /* ADC1 RAM */
             | (uint32)0x00000000U    /* ADC2 RAM */
             | (uint32)0x00000000U    /* HET1 RAM */
             | (uint32)0x00000000U    /* HET2 RAM */
             | (uint32)0x00000000U    /* HTU1 RAM */
             | (uint32)0x00000000U    /* HTU2 RAM */
             | (uint32)0x00004000U    /* RTP RAM */
             | (uint32)0x00000000U    /* FRAY RAM */
             ,(uint32) PBIST_March13N_DP);

/* USER CODE BEGIN (40) */
/* USER CODE END */

    /* Test the CPU ECC mechanism for RAM accesses.
     * The checkBxRAMECC functions cause deliberate single-bit and double-bit errors in TCRAM accesses
     * by corrupting 1 or 2 bits in the ECC. Reading from the TCRAM location with a 2-bit error
     * in the ECC causes a data abort exception. The data abort handler is written to look for
     * deliberately caused exception and to return the code execution to the instruction
     * following the one that caused the abort.
     */
    checkRAMECC();

/* USER CODE BEGIN (41) */
/* USER CODE END */

    /* Test the CPU ECC mechanism for Flash accesses.
     * The checkFlashECC function uses the flash interface module's diagnostic mode 7
     * to create single-bit and double-bit errors in CPU accesses to the flash. A double-bit
     * error on reading from flash causes a data abort exception.
     * The data abort handler is written to look for deliberately caused exception and
     * to return the code execution to the instruction following the one that was aborted.
     *
     */
    checkFlashECC();
    flashWREG->FDIAGCTRL = 0x000A0007U;                    /* disable flash diagnostic mode */

/* USER CODE BEGIN (42) */
/* USER CODE END */

/* USER CODE BEGIN (43) */
/* USER CODE END */

    /* Wait for PBIST for CPU RAM to be completed */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
    while(pbistIsTestCompleted() != TRUE)
    { 
    }/* Wait */                 
    

/* USER CODE BEGIN (44) */
/* USER CODE END */

    /* Check if CPU RAM passed the self-test */
    if( pbistIsTestPassed() != TRUE)
    {

/* USER CODE BEGIN (45) */
/* USER CODE END */

        /* CPU RAM failed the self-test.
         * Need custom handler to check the memory failure
         * and to take the appropriate next step.
         */
/* USER CODE BEGIN (46) */
/* USER CODE END */
         
        pbistFail();
        
/* USER CODE BEGIN (47) */
/* USER CODE END */
    }

/* USER CODE BEGIN (48) */
/* USER CODE END */

    /* Disable PBIST clocks and disable memory self-test mode */
    pbistStop();
    
/* USER CODE BEGIN (55) */
/* USER CODE END */

/* USER CODE BEGIN (56) */
/* USER CODE END */

    /* Enable parity on selected RAMs */
    enableParity();
    
    /* Initialize all on-chip SRAMs except for MibSPIx RAMs
     * The MibSPIx modules have their own auto-initialization mechanism which is triggered
     * as soon as the modules are brought out of local reset.
     */
    /* The system module auto-init will hang on the MibSPI RAM if the module is still in local reset.
     */
    /* NOTE : Please Refer DEVICE DATASHEET for the list of Supported Memories and their channel numbers.
              Memory Initialization is perfomed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
     */
    memoryInit( (uint32)((uint32)1U << 1U)    /* DMA RAM */
              | (uint32)((uint32)1U << 2U)    /* VIM RAM */
              | (uint32)((uint32)0U << 5U)    /* CAN1 RAM */
              | (uint32)((uint32)0U << 6U)    /* CAN2 RAM */
              | (uint32)((uint32)0U << 10U)   /* CAN3 RAM */
              | (uint32)((uint32)0U << 8U)    /* ADC1 RAM */
              | (uint32)((uint32)1U << 14U)   /* ADC2 RAM */
              | (uint32)((uint32)0U << 3U)    /* HET1 RAM */
              | (uint32)((uint32)0U << 4U)    /* HTU1 RAM */
              | (uint32)((uint32)0U << 15U)   /* HET2 RAM */
              | (uint32)((uint32)0U << 16U)   /* HTU2 RAM */
              );

    /* Disable parity */
    disableParity();
    
    /* Test the parity protection mechanism for peripheral RAMs
       NOTE : Please Refer DEVICE DATASHEET for the list of Supported Memories with parity.
                 Parity Self check is perfomed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
    */

/* USER CODE BEGIN (62) */
/* USER CODE END */

    adc2ParityCheck();
    
/* USER CODE BEGIN (66) */
/* USER CODE END */

    vimParityCheck();
    
/* USER CODE BEGIN (67) */
/* USER CODE END */

    dmaParityCheck();


/* USER CODE BEGIN (68) */
/* USER CODE END */



/* USER CODE BEGIN (72) */
/* USER CODE END */
    
    /* Enable IRQ offset via Vic controller */
    _coreEnableIrqVicOffset_();
    

/* USER CODE BEGIN (73) */
/* USER CODE END */

    /* Initialize VIM table */
    vimInit();    

/* USER CODE BEGIN (74) */
/* USER CODE END */

    /* Configure system response to error conditions signaled to the ESM group1 */
    /* This function can be configured from the ESM tab of HALCoGen */
    esmInit();
    /* initialize copy table */
    __TI_auto_init();
/* USER CODE BEGIN (75) */
/* USER CODE END */
    
    /* call the application */
/*SAFETYMCUSW 296 S MR:8.6 <APPROVED> "Startup code(library functions at block scope)" */
/*SAFETYMCUSW 326 S MR:8.2 <APPROVED> "Startup code(Declaration for main in library)" */
/*SAFETYMCUSW 60 D MR:8.8 <APPROVED> "Startup code(Declaration for main in library;Only doing an extern for the same)" */
    main();

/* USER CODE BEGIN (76) */
/* USER CODE END */
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
    exit(0);

/* USER CODE BEGIN (77) */
/* USER CODE END */
}

/* USER CODE BEGIN (78) */
/* USER CODE END */
  How should I go about changing sys_startup.c file according the reply in the thread mentioned:

  • When going through the initialization of the microcontroller, be careful with steps such as CPU RAM auto-initialization or CPU RAM self-test using PBIST. These must be disabled for the CPU RAM, else they will cause the application to crash (run NOPs).

  • Lakshit,

    I wouldn't worry about the write erase cycles on a development board that is going to sit on your desk. Yes the spec in the datasheet is pretty low but it is somewhat conservative and assumes worst case scenarios like you are erasing at very cold temperatures and you expect the flash to retain values without error for the lifetime of the part.

    I can tell you that I've got the same development kits that I had several years ago and have yet to wear out the flash using them daily.

    What you are asking to do by relocating the whole program intended for flash to SRAM can be done but as you've found you'll need to do a lot of work on your own modifying the startup code - because the startup code both initializes and tests the SRAM. Neither of these will work correctly if the code that launches them is running from SRAM.

    In my opinion - it makes zero sense to go through this effort when you can buy another launchpad for $29 if you happen to wear a part out - and when you probably will never wear a part out that is just sitting on your desk.

    HalCoGen doesn't support this use model so it'll take you tens of hours to figure it out - and that doesn't make sense relative to the price of a new dev. kit.

    Just my opinion - but it's definitely what I would do.

    Best Regards,
    Anthony