Other Parts Discussed in Thread: RM48L530, RM48L950
Hello, I have a question about SafeTI Diagnostic Library module project. I download the "SL_RM48L950_NoOS" from TI website and try to run it on the RM48L530. However, I find the Flash and Ram size are different between cpu 950(3Mb and 256Kb) and 530(2Mb and 192Kb). When I run the project in the 530, the program will fall into the endless loop at the line 596 of the "sys_startup.c",as flowing grahp:
/* Get SRAM PBIST Status */
SL_SelfTest_Status_PBIST(&failInfoPBISTSRAM);
if (failInfoPBISTSRAM.stResult == ST_PASS) {
initSTPassCount++;
} else {
initSTFailCount++;
for(;;)
{
}/* Wait */
}
The pbist selftest always return the value of "0xAB".
Hence, I modify the "memory map" which in the document "SL_RM48L950_NoOS_sys_link.cmd". It was as below:
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00001800
RAM (RW) : origin=0x08008000 length=0x00028000
PROFILE(RW) : origin=0x08036000 length=0x00008000 /* Added for profiling purposes */
LOG (RW) : origin=0x080053B0 length=0x00002000 fill=0xDEADBEEF/* Added for logging purposes */
FEE (R) : origin=0xF0200000 length=0x00000064 fill=0xDEADBEEF /* For FEE testing, Valid only for sample application */
}
Now, after calculating, I have modified like following:
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x000FFFE0
FLASH1 (RX) : origin=0x00100000 length=0x00100000
STACKS (RW) : origin=0x08000000 length=0x00001800
RAM (RW) : origin=0x08008000 length=0x00018000
PROFILE(RW) : origin=0x08026000 length=0x00008000 /* Added for profiling purposes */
LOG (RW) : origin=0x080053B0 length=0x00002000 fill=0xDEADBEEF/* Added for logging purposes */
FEE (R) : origin=0xF0200000 length=0x00000064 fill=0xDEADBEEF /* For FEE testing, Valid only for sample application */
}
The program can be bulit successfully, but it falls into the endless loop at the line 596 of "startup.c" as before. Can you tell me that how to modify the project. Do I need modify it anymore?