Hi,
Im trying to have the MPU 6050 IMU sensor interfaced through I2C communication. My problem is when going through the setup process as outlined in the data sheet, the I2C1_MDR_R register is always zero or always 255.
Here's my code
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "sensorlib/hw_mpu9150.h"
#include "sensorlib/hw_ak8975.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/ak8975.h"
#include "sensorlib/mpu9150.h"
#include "sensorlib/comp_dcm.h"
#include "sensorlib/hw_mpu6050.h"
#include "inc/tm4c123gh6pm.h"
int main(void) {
uint32_t acc_x_L=0;
while(1){
//16.4.1 Configure the I2C Module to Transmit a Single Byte as a Master
//The following example shows how to configure the I2C module to transmit a single byte as a master.
//This assumes the system clock is 20 MHz.
//1. Enable the I2C clock using the RCGCI2C register in the System Control module (see page 348).
SYSCTL_RCGCI2C_R=(1<<1);//selected i2c module 1 (will connect to portA pin 6 and 7 with I2C1_SCL and I2C1_SDA respectively
//2. Enable the clock to the appropriate GPIO module via the RCGCGPIO register in the System
//Control module (see page 340). To find out which GPIO port to enable, refer to Table
//23-5 on page 1351.
SYSCTL_RCGCGPIO_R=(1<<0);//Clock to port A (pin 6 and 7 will have I2C1_SCL and I2C1_SDA respectively)
//3. In the GPIO module, enable the appropriate pins for their alternate function using the
//GPIOAFSEL register (see page 671). To determine which GPIOs to configure, see Table
///23-4 on page 1344.
GPIO_PORTA_AFSEL_R=0xC0;//pin 6 and 7 are assigned alternative function. Nanmely connecting to I2C1_SCL and I2C1_SDA respectively
GPIO_PORTA_DEN_R=0b11000000;//set pin 6 and 7 to be digitcal pins
GPIO_PORTA_PUR_R=0b11000000;//SDA and SCL pulled up
//4. Enable the I2CSDA pin for open-drain operation. See page 676.
GPIO_PORTA_ODR_R=0b10000000;//set SDA pin to open drain (bit 7 (pin 8) is set to high)
//5. Configure the PMCn fields in the GPIOPCTL register to assign the I2C signals to the appropriate
//pins. See page 688 and Table 23-5 on page 1351.
GPIO_PORTA_PCTL_R=(0x33 <<24);
//6. Initialize the I2C Master by writing the I2CMCR register with a value of 0x0000.0010.
I2C1_MCR_R=0x10;
//7. Set the desired SCL clock speed of 100 Kbps by writing the I2CMTPR register with the correct
//value. The value written to the I2CMTPR register represents the number of system clock periods
//in one SCL clock period. The TPR value is determined by the following equation:
//TPR = (System Clock/(2*(SCL_LP + SCL_HP)*SCL_CLK))-1;
//TPR = (16MHz/(2*(6+4)*100000))-1;
//TPR = 7
//Write the I2CMTPR register with the value of 0x0000.0007.
I2C1_MTPR_R=0x9;
//8. Specify the slave address of the master and that the next operation is a Transmit by writing the
//I2CMSA register with a value of 0x0000.0076. This sets the slave address to 0x3B.
I2C1_MSA_R=(0x68 <<1 & 0xFE);// send
//9. Place data (byte) to be transmitted or recived in the data register by writing the I2CMDR register with the
//desired data.
I2C1_MDR_R= 0x3C;//write the register to read from
//10. Initiate a single byte transmit of the data from Master to Slave by writing the I2CMCS register
//with a value of 0x0000.0007 (STOP, START, RUN).
I2C1_MCS_R=0b00000011;
//11. Wait until the transmission completes by polling the I2CMCS register's BUSBSY bit until it has
//been cleared.
while(I2C1_MCS_R & 0b00000001 !=0);
I2C1_MCS_R=0b00001011;
// Wait while i2c module is not busy
//while(!(I2C1_MCS_R & 0b00000001 !=0))
I2C1_MSA_R=(0x68<<1 | 0x01);// recieve
//12. Check the ERROR bit in the I2CMCS register to confirm the transmit was acknowledged.
while (I2C1_MCS_R & 0x02 != 0);
}
return 0;
}
Mind you I am forced to code everything in registers so I cant code anything using the pre defined libraries.
Your help will be appreciated,