Other Parts Discussed in Thread: TM4C1294NCPDT
Hi
I am very new to the TI microcontrollers. Have a TM4C1294XL Launchpad and I have just started with the example applications. I tested the uart_echo example on the board.
Now I have just started a new project in the CCS and in the main.c, just copied all the code from the uart_echo example c file and I am trying to run that.
First problem i faced was regarding the files in #include. So I added the respective paths in include options in my project settings.
Further, I see a lot of errors and warnings on this new project.
Description Resource Path Location Type
#10010 errors encountered during linking; "mytrials1.out" not built mytrials1 C/C++ Problem
#10234-D unresolved symbols remain mytrials1 C/C++ Problem
unresolved symbol GPIOPinConfigure, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol GPIOPinWrite, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_GPIOPinTypeGPIOOutput, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_GPIOPinTypeUART, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_IntEnable, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_IntMasterEnable, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_SysCtlPeripheralEnable, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTCharGetNonBlocking, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTCharPutNonBlocking, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTCharsAvail, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTConfigSetExpClk, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTIntClear, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTIntEnable, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol ROM_UARTIntStatus, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol SysCtlClockFreqSet, first referenced in ./main.obj mytrials1 C/C++ Problem
unresolved symbol SysCtlDelay, first referenced in ./main.obj mytrials1 C/C++ Problem
#225-D function "ROM_GPIOPinTypeGPIOOutput" declared implicitly main.c /mytrials1 line 175 C/C++ Problem
#225-D function "ROM_GPIOPinTypeUART" declared implicitly main.c /mytrials1 line 194 C/C++ Problem
#225-D function "ROM_IntEnable" declared implicitly main.c /mytrials1 line 206 C/C++ Problem
#225-D function "ROM_IntMasterEnable" declared implicitly main.c /mytrials1 line 187 C/C++ Problem
#225-D function "ROM_SysCtlPeripheralEnable" declared implicitly main.c /mytrials1 line 169 C/C++ Problem
#225-D function "ROM_UARTCharGetNonBlocking" declared implicitly main.c /mytrials1 line 99 C/C++ Problem
#225-D function "ROM_UARTCharPutNonBlocking" declared implicitly main.c /mytrials1 line 109 C/C++ Problem
#225-D function "ROM_UARTCharPutNonBlocking" declared implicitly main.c /mytrials1 line 147 C/C++ Problem
#225-D function "ROM_UARTCharsAvail" declared implicitly main.c /mytrials1 line 94 C/C++ Problem
#225-D function "ROM_UARTConfigSetExpClk" declared implicitly main.c /mytrials1 line 199 C/C++ Problem
#225-D function "ROM_UARTIntClear" declared implicitly main.c /mytrials1 line 89 C/C++ Problem
#225-D function "ROM_UARTIntEnable" declared implicitly main.c /mytrials1 line 207 C/C++ Problem
#225-D function "ROM_UARTIntStatus" declared implicitly main.c /mytrials1 line 84 C/C++ Problem
What more am I required to do in order to build and run this on the board? What more steps am I missing?
Regards
KK