Other Parts Discussed in Thread: TMS570LS1227
Hello,
I have a problem about debug session on Code Composer Studio.
When I tried to execute debug session on Code Composer Studio ( version 5.3.0), the error code shown :
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: GEL: File: C:\XXXXXXXX.out Does not match the target endianness, not loaded. Check build options and target configuration file (ccxml).
CortexR4: Trouble Reading Register REG_ENDIAN: (Error -150 @ 0x88) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.0.872.0)
CortexR4: Trouble Reading Register REG_ENDIAN: (Error -1044 @ 0xFFFFFF0E) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.872.0)
I could execute the debug session normally when one year ago , using the same CCS and the same CCS project,and the same custom board.
And I have no idea if the endianness is correct or not.(I didn't see the error message when tryied to do it on one year ago)
The MCU is Hercules TMS570LS1227,and the debugger is XDS100V2 ( with FTDI chip FT2232H).
And the PC OS is Windows7 64bit.
Could someone reply to my question ?
I would appriciate if someone could reply.
Regards,
Hiroyasu