Other Parts Discussed in Thread: TM4C123GH6PM
Hello guys,
I am using TM4C123GH6PM . while dump a application into controller normally it happens .but once i dump application with PLL active after that ..
most of the times it fails with the below message....
CORTEX_M4_0: Can' Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
CORTEX_M4_0: Flash Programmer: Error while writing to Flash memory
CORTEX_M4_0: File Loader: Memory write failed: Unknown error
CORTEX_M4_0: GEL: File:
am using ..XDS100V2 usb debug probe....
int main(void) {
ROM_FPUEnable();
ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4| SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
while (1) {
ROM_UARTCharPut(UART0_BASE, 'A');
}
}
please let me know how to resolve this issue....