Hello everyone,
It's my first time asking a question here, I design a custom pcb for a school project, but I have solder at least 4 MCUs in the board with no success, I have tried with solder wire but I think the temperature is too high with the soldering pencil, then I tried with hot air at 150° but it seems not to work very well with the solder paste I have. I just populated a 3.3v regulator, some decoupling caps, and the caps for VDDC, when I energize the board the VDDC voltage is too low, no voltage in my opinion, and the LM Flash programmer as the CCS are unable to detect my board (JTAG interface with a launchpad).
I really would like to know what technique and materials are used in populating the tm4c123gh6pmi in the launchpad, or what do you recommend me to get my system working.
Thank you very much.