This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not able to erase programTM4c1290NCPDT



Hi,

Microcontroller :-TM4C1290NCPDT

IDE    :-CCS 6.0.1

Debugger :-XDS 100v2

Programmer:-Mikroprog

 

Code is written to test the WDT2,for this we have enabled WDT2 with some millisecond

and it is configured for RESET. WDT interrupt reset function is disabled to check the delay.

              Now the problem is we are not able to erase or reprogram the microcontroller using Debugger or using programmer because of frequent resetting of controller by WDT.

Please suggest how will I erase or reprogram the device

Regards,

yash