I am using the TM4C129EKCPDT microprocessor with an external 32.768kHz crystal (20ppm). It is the same crystal that is used on the TM4C development board. Currently we are not doing any calibration and are seeing an inaccuracy of 3.5 secs/day.
What can be done to improve this drift? Or is this the best we can achieve based on the characteristics of the crystal?
Thank you.