This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SSI2 and SSI3 outputs on DK-TM4C129X

I wanted to use two SSI modules on my DK-TM4C129X board. The first SSI would act as a master and the second one as a slave.

First I've decided to init all of SSI modules to chek: which of them have all the outputs on BoosterPack pin headers for interconnection one module to another.

I setup all SSI with such code:

//SSI0 - TX
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
    GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);//GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);//GPIO_PA5_SSI0TX);

    GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |
                   GPIO_PIN_2);

#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    SSIConfigSetExpClk(SSI0_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#else
    SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#endif

    //
    // Enable the SSI0 module.
    //
    SSIEnable(SSI0_BASE);

// SSI1 - TX
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

    GPIOPinConfigure(GPIO_PB5_SSI1CLK);
    GPIOPinConfigure(GPIO_PB4_SSI1FSS);
    GPIOPinConfigure(GPIO_PE4_SSI1XDAT0);//TX);
    GPIOPinConfigure(GPIO_PE5_SSI1XDAT1);//RX);

    GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    GPIOPinTypeSSI(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5);

#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    SSIConfigSetExpClk(SSI1_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#else
    SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_SLAVE, 1000000, 8);
#endif

    SSIEnable(SSI1_BASE);

// SSI2 - TX
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);

    GPIOPinConfigure(GPIO_PD3_SSI2CLK);
    GPIOPinConfigure(GPIO_PD2_SSI2FSS);
    GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);	// RX
    GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);	// RX
    GPIOPinConfigure(GPIO_PG4_SSI2XDAT1);	// TX

    GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
    GPIOPinTypeSSI(GPIO_PORTG_BASE, GPIO_PIN_4);

#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    SSIConfigSetExpClk(SSI2_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#else
    SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#endif

    SSIEnable(SSI2_BASE);

//SSI3 - TX
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);

    GPIOPinConfigure(GPIO_PF3_SSI3CLK);
    GPIOPinConfigure(GPIO_PF2_SSI3FSS);
    GPIOPinConfigure(GPIO_PF0_SSI3XDAT1);//TX);
    GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);//TX);
    GPIOPinConfigure(GPIO_PF1_SSI3XDAT0);//RX);

    GPIOPinTypeSSI(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 );
    GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_3 );

#if defined(TARGET_IS_TM4C129_RA0) ||                                         \
    defined(TARGET_IS_TM4C129_RA1) ||                                         \
    defined(TARGET_IS_TM4C129_RA2)
    SSIConfigSetExpClk(SSI3_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER, 1000000, 8);
#else
    SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_SLAVE, 1000000, 8);
#endif
 
   SSIEnable(SSI3_BASE);

Further I just send some symbols thru each SSI in endless loop:

while(1){
// SSI0 - PA5. Send 3 bytes of data.
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
    }
    while(SSIBusy(SSI0_BASE)){}

// SSI1 - PE4. Send 3 bytes of data.
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        SSIDataPut(SSI1_BASE, pui32DataTx[ui32Index]);
    }
    while(SSIBusy(SSI1_BASE)){}

// SSI2 - PD0/PG4. Send 3 bytes of data.
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        SSIDataPut(SSI2_BASE, pui32DataTx[ui32Index]);
    }
    while(SSIBusy(SSI2_BASE)){}

// SSI3 - PF0/PQ3. Send 3 bytes of data.
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        SSIDataPut(SSI3_BASE, pui32DataTx[ui32Index]);
    }
    while(SSIBusy(SSI3_BASE)){}
}

When I check SSI outputs with scope, I see the next activity:

SSI0 - PA5 - Activity is present

SSI1 - PE4 - Activity is present

SSI2 - PD0/PG4 - No activity

SSI3 - PF0/PQ3 - No activity

So the question is: How can I use SSI2 and SSI3 on my DK-TM4C129X board? What I've missed?

  • Hello Vyacheslav

    The SSI3 instance is used for the SD Card and QSSI flash on the DK-TM4C129X and it is a tested interface for the example code. Have you made sure that the jumpers have been removed?

    Did you check the clock pins and FSS pins on the respective modules for activity? Do make sure that there are no other jumpers connected on the board when probing the clock and FSS pins.

    Regards
    Amit