Hello
I want to merge by button interrupt project with a "hello world" lcd example. It should be straight forward as neither program changes, just shares the same main method. Everything compiles fine and the LCD display works, but my button interrupts (which toggle the onboard LEDs) no longer work. I've tried this in both CCS and uVision4.
Even after I edit out all of the code associated with the LCD my buttons still do not work.
Any advice?
//*****************************************************************************
//
// scribble.c - A simple scribble pad to demonstrate the touch screen driver.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_memmap.h"
#include "driverlib/flash.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"
#include "driverlib/interrupt.h"
#include "grlib/grlib.h"
#include "grlib/widget.h"
#include "utils/ringbuf.h"
#include "utils/ustdlib.h"
#include "inc/hw_gpio.h"
#include "inc/tm4c123gh6pm.h"
#include "drivers/Kentec320x240x16_ssd2119_8bit.h"
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
//
// The graphics context used by this application.
//
//*****************************************************************************
tContext g_sContext;
volatile unsigned long counter = 0;
void
PortFunctionInit(void)
{
//
// Enable Peripheral Clocks
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable pin PF2 for GPIOOutput
//
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
//
// Enable pin PF0 for GPIOInput
//
//
//First open the lock and select the bits we want to modify in the GPIO commit register.
//
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) = 0x1;
//
//Now modify the configuration of the pins that we unlocked.
//
GPIOPinTypeGPIOInput(GPIO_PORTF_BASE, GPIO_PIN_0);
//
// Enable pin PF4 for GPIOInput
//
GPIOPinTypeGPIOInput(GPIO_PORTF_BASE, GPIO_PIN_4);
//
// Enable pin PF1 for GPIOOutput
//
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1);
//Enable pull-up on PF0 and PF4 (switch2 and switch1)
GPIO_PORTF_PUR_R |= 0x11; // decimal 17 to turn on
//GPIO_PORTF_PUR_R |= 0x01;
}
//////////////////////////////////////////////////
void
Interrupt_Init(void)
{
IntEnable(INT_GPIOF); // enable interrupt 30 in NVIC (GPIOF)
IntPrioritySet(INT_GPIOF, 0x00); // configure GPIOF interrupt priority as 0
GPIO_PORTF_IM_R |= 0x11; // arm interrupt on PF0 and PF4
GPIO_PORTF_IS_R &= ~0x11; // PF0 and PF4 are edge-sensitive
GPIO_PORTF_IBE_R &= ~0x11; // PF0 and PF4 not both edges trigger
GPIO_PORTF_IEV_R &= ~0x11; // PF0 and PF4 falling edge event
IntMasterEnable(); // globally enable interrupt
}
/////////////////////////////////////////////////////////
//interrupt handler
void GPIOPortF_Handler(void)
{
//debounce
IntDisable(INT_GPIOF);//disable inturrupt
SysCtlDelay(53333333);//short delay
IntEnable(INT_GPIOF);
//SW1 is pressed (if flag recieved)
if(GPIO_PORTF_RIS_R&0x10 )
{
// acknowledge flag for PF4
GPIOIntClear(GPIO_PORTF_BASE, GPIO_PIN_4);
//counter incremented by 1
counter=counter+1;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //blue on
}
//SW2 is pressed (if flag recieved)
if(GPIO_PORTF_RIS_R&0x01 )
{
// acknowledge flag for PF0
GPIOIntClear(GPIO_PORTF_BASE, GPIO_PIN_0);
//counter decremented by 1
counter--;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //blue on
}
}
//////////////////////////////////////////
//*****************************************************************************
//
// Print "Hello World!" to the display on the Intelligent Display Module.
//
//*****************************************************************************
int
main(void)
{
//tRectangle sRect;
PortFunctionInit();
Interrupt_Init();
//
// Set the clocking to run directly from the crystal.
//
/*
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Initialize the display driver.
//
Kentec320x240x16_SSD2119Init();
//
// Initialize the graphics context.
//
GrContextInit(&g_sContext, &g_sKentec320x240x16_SSD2119);
//
// Fill the top 24 rows of the screen with blue to create the banner.
//
sRect.i16XMin = 0;
sRect.i16YMin = 0;
sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - 1;
sRect.i16YMax = 23;
GrContextForegroundSet(&g_sContext, ClrDarkBlue);
GrRectFill(&g_sContext, &sRect);
//
// Put a white box around the banner.
//
GrContextForegroundSet(&g_sContext, ClrWhite);
GrRectDraw(&g_sContext, &sRect);
//
// Put the application name in the middle of the banner.
//
GrContextFontSet(&g_sContext, &g_sFontCm20);
GrStringDrawCentered(&g_sContext, "hello", -1,
GrContextDpyWidthGet(&g_sContext) / 2, 11, 0);
//
// Say hello using the Computer Modern 40 point font.
//
GrContextFontSet(&g_sContext, &g_sFontCm40);
GrStringDrawCentered(&g_sContext, "Hello World!", -1,
GrContextDpyWidthGet(&g_sContext) / 2,
((GrContextDpyHeightGet(&g_sContext) - 24) / 2) + 24,
0);
//
// The boot loader should take control, so this should never be reached.
// Just in case, loop forever.
*/
//
while(1)
{
// GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //blue on
//GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1,0x02); //red on
if (counter==0)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00); //blue off
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1,0x00); //red off
}
if (counter==1)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00); //blue off
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1,0x02); //red on
}
if (counter==2)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //blue on
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1,0x00); //red off
}
if (counter==3)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //blue on
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1,0x02); //red on
}
if (counter>3)
counter=0; //counter reset
}
}