Other Parts Discussed in Thread: RM57L843, HALCOGEN, TMS570LC4357
Hi,
we are finding a discrepancy between the RM57L843 TRM Table 7-12 and the Halcogen header file HL_reg_flash.h.
Some of the reserved spacing seems to have the wrong rsvd[] array length.
If the Table 7-12 is correct then
uint32 rsvd14[109U]; /* 0x00D8 - 0x00284 */
needs to be
uint32 rsvd14[108U]; /* 0x00D8 - 0x00284 */
uint32 rsvd15[12U]; /* 0x028C - 0x002B4 */
needs to be
uint32 rsvd15[11U]; /* 0x028C - 0x002B4 */
uint32 rsvd17[79U]; /* 0x02A8 */
needs to be
uint32 rsvd17[78U]; /* 0x02A8 */
Additionally the file seems to be pulled from
C:\TI\Hercules\HALCoGen\v04.05.02\drivers\TMS570LC4357ZWT\SYSTEM570v000\reg_flash.h
And I want to make sure the register mapping is the same for that device.
Regards,
--Gunter