Hi,
I am using RM46 Hercules development kit. I see from its board manual that switch S2 controls the ennoblement of peripherals. peripherals corresponds to certain groups as Switched central Resource, Peripherals central Resource group. Some peripherals like UART, SPI corresponds to one group and require S2 be in one state. Ethernet requires S2 in an other state and USB requires S2 in a 3rd configuration. It means all these three groups can not work simultaneously. I have also practically observed the Uart and Ethernet do not work simultaneously if Switch corresponds to Ethernet requirement. Can you please confirm this behavior? If I want to use all devices at ones, is there any workaround available for this platform.
Thanks in advance,
JA