Concerning the TMS570LS20216, please answer the following questions:
- ATCM Configuration. I think the flash is connected to this, but not sure.
- BTCM Configuration. According to TRM, the silicon is configured for two-banked BTCM, with half the the RAM on each bank, correct?
- Instruction Cache. I can't tell if the silicon has no cache or it does have cache but not documented.
- Data Cache. I can't tell if the silicon has no cache or it does have cache but not documented.
- What is the wait-state for the RAM and FLASH? Please describe for each.
- Are there any additional wait-states for ECC? Please describe.