Hello team TI
What is the location of PBIST ROM and STC(1 and 2) ROMs in TMS570LC4357?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team TI
What is the location of PBIST ROM and STC(1 and 2) ROMs in TMS570LC4357?
Hello Anthony
I would like to get cleared a few doubts I have on Safety Library example Code provided in HalCoGen for TMS570LC4357.
1) After loading the program, I see the following status in the ESM register
Why does these errors are indicated in Status registers 1,4 and Shadow Status 2 registers ?
2) Why ESM Initialization is done after PBIST test?
3) If ESM Init(); is called before the Errata Workaround ( errata_PBIST_4() ) provided in Example code, the ErrPinStat register remains 0x00000000 and doesn't return to 0x00000001 as expected (because ErrKey=0x05 is written in esminit() ), whereas all other Status registers are reset ?
4) Please let me know if these error status is related to the device errata #48 an #49 of Silicon Revision B.
Thanks in advance.