Other Parts Discussed in Thread: LM3S8962, EK-TM4C1294XL
Hi Community,
I bought a stellaris EKS-LM3S8962 EVALUATION KIT.
My project requires me to do digital signal processing.
My question to the community is that, for the LM3S8962 micro-controller board, there are many pins on the board that labelled as gnd and vcc. If I wish to do any forms of soldering on the board, can I just connect to any gnd pin and it will work? I bought a electret microphone amplifier which has out,gnd,vcc pins. I have to create a connection between the mic and the micro-controller board. As such, does it have any difference if i just choose any pin that labelled as gnd and just solder them and create the connectivity? On the board itself, all the pins that labelled gnd are the same right? I can just solder to any gnd?