Other Parts Discussed in Thread: EK-TM4C129EXL
Hello,
I'm a beginner using the board Tiva C series EK-TM4C129EXL.
I need to use the ADC so in order to check my configuration, I use the UART to send the results.
I have 5 sensors and I need to sample their signal with a sampling frequency of 100kHz. In my code, I try to do it this way:
- Sample from pin PE0 with ADC0, sample sequencer SS2, first.
- Sample from pin PE0 with ADC0, sample sequencer SS2, second.
- Sample from pin PE0 with ADC0, sample sequencer SS2, last.
For the last 2 sensors, I need to synchronize twice of their samples (2 samples for each sensor) so:
- Sample from pin PE3 with ADC0, sample sequencer SS0, sync. with sample from pin PE5 with ADC1, sample sequencer SS0,
- Sample from pin PE3 with ADC0, sample sequencer SS0, a second time sync. with sample from pin PE5 with ADC1, sample sequencer SS0 a second time
For the moment, I haven't got any input (0V) so the UART should send 0. The timer frequency is set to 5 HZ for the UART.
Here is my code (Sorry for the french commentary, I can translate if it's necessary but I think the code is understandable like this)
#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/adc.h"
#include "drivers/pinout.h"
#include "Custom files/constantes.h"
#include "Custom files/maths.h"
#include "Custom files/fichier.h"
// System clock rate in Hz.
uint32_t g_ui32SysClock;
// The error routine that is called if the driver library encounters an error.
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//
// Définition des variables utiles
//
#define TMR0_FREQ 5 //Hz //100000 //Hz
uint8_t LED = 0;
uint32_t ADCbuffer[3], thetaSinBuffer[3], thetaCosBuffer[3];
// Configuration des ADC
void
ConfigureADC(void)
{
UARTprintf("Configuration des ADC\n");
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
ADCReferenceSet(ADC1_BASE, ADC_REF_INT);
GPIOPinTypeADC(GPIO_PORTE_BASE,GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_5);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0) && !SysCtlPeripheralReady(SYSCTL_PERIPH_ADC1) && !SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE))
{}
UARTprintf("ADC et ports I/O autorisés\n");
////// Désactivation des ADC (sécurité)
ADCSequenceDisable(ADC0_BASE,2);
ADCSequenceDisable(ADC0_BASE,0);
ADCSequenceDisable(ADC1_BASE,0);
UARTprintf("Séquenceurs ADC désactivés\n");
////// Configuration des ADC
// Séquence courant -> température -> potentiomètre
ADCSequenceConfigure(ADC0_BASE,2,ADC_TRIGGER_PROCESSOR,0); //ADC0 Sequence 2 déclenchement processeur priorité 0 (Haute)
UARTprintf("Configuration 1 finie\n");
//positionSin et positionCos sync
ADCSequenceConfigure(ADC0_BASE,0,ADC_TRIGGER_PROCESSOR,0);
ADCSequenceConfigure(ADC1_BASE,0,ADC_TRIGGER_PROCESSOR,0);
UARTprintf("Configuration des ADC finie\n");
////// Configuration des séquences
// Séquence courant -> température -> potentiomètre
ADCSequenceStepConfigure(ADC0_BASE,2,0,ADC_CTL_CH1); //Courant
ADCSequenceStepConfigure(ADC0_BASE,2,1,ADC_CTL_CH2); //Température
ADCSequenceStepConfigure(ADC0_BASE,2,2,ADC_CTL_CH3|ADC_CTL_IE|ADC_CTL_END); //Potentiomètre
// positionSin et positionCos sync
// séquence de 2 échantillons pour la dérivée
ADCSequenceStepConfigure(ADC0_BASE,0,0,ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE,0,1,ADC_CTL_CH0|ADC_CTL_IE|ADC_CTL_END);
ADCSequenceStepConfigure(ADC1_BASE,0,0,ADC_CTL_CH8);
ADCSequenceStepConfigure(ADC1_BASE,0,1,ADC_CTL_CH8|ADC_CTL_IE|ADC_CTL_END);
UARTprintf("Configurations des séquences\n");
////// Activations des ADC
ADCSequenceEnable(ADC0_BASE,2);
ADCSequenceEnable(ADC0_BASE,0);
ADCSequenceEnable(ADC1_BASE,0);
UARTprintf("Activation des ADC\n");
// Reset des flags d'interuption des ADC
ADCIntClear(ADC0_BASE,2);
ADCIntClear(ADC0_BASE,0);
ADCIntClear(ADC1_BASE,0);
}
//
// Fonction d'interuption du timer 0
//
void
Timer0IntHandler(void)
{
// Reset le flag de l'interuption du timer
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
////// ADC
// initialise le flag de l'interuption de l'ADC
ADCIntClear(ADC0_BASE,2);
// Déclenche la conversion
ADCProcessorTrigger(ADC0_BASE,2);
while(!ADCIntStatus(ADC0_BASE,2,false)){} // attend la fin de la conversion
// Reste le flag de l'interuption de l'ADC
ADCIntClear(ADC0_BASE,2);
// Lecture des données
ADCSequenceDataGet(ADC0_BASE,2,ADCbuffer);
UARTprintf("Sequence: %d %d %d\n",ADCbuffer[0],ADCbuffer[1],ADCbuffer[2]);
// position, sync
ADCIntClear(ADC0_BASE,0);
ADCIntClear(ADC1_BASE,0);
// déclenche les conversions synchronisées
ADCProcessorTrigger(ADC1_BASE,(0|ADC_TRIGGER_WAIT)); // ADC-1 en attente de déclenchement
ADCProcessorTrigger(ADC0_BASE,(0|ADC_TRIGGER_SIGNAL)); // ADC-0 en déclenchement global
while(!ADCIntStatus(ADC0_BASE,0,false)){} // attend la fin de la conversion
// Reset le flag de l'interuption de l'ADC
ADCIntClear(ADC0_BASE,0);
ADCIntClear(ADC1_BASE,0);
// Lecture des données
ADCSequenceDataGet(ADC0_BASE,0,thetaSinBuffer);
ADCSequenceDataGet(ADC1_BASE,0,thetaCosBuffer);
UARTprintf("Sync.: %d %d %d %d\n",thetaSinBuffer[0],thetaSinBuffer[1],thetaCosBuffer[0],thetaCosBuffer[1]);
//test: la diode s'allume si le timer a le temps d'aller au bout
HWREGBITW(&LED, 0) ^= 1; // (bit 0 du registre de LED) XOR 1
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, LED);
}
// Initialise le port série. Doit être appellée avant UARTprintf().
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, CLP_D2_PIN | CLP_D1_PIN);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, g_ui32SysClock);
}
////// Set up, loop forever
int
main(void)
{
////// Set up
// Règle l'horloge sur le cristal à 120MHz
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
// Initialisation du port série
ConfigureUART();
UARTprintf("GO! \n");
// Active le port des diodes
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPION)){}
GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, LED); // LED = 0
// Active le périphérique Timer 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
// Enable processor interrupts
IntMasterEnable();
// Configure the 32-bit periodic timers.
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
TimerLoadSet(TIMER0_BASE, TIMER_A, g_ui32SysClock/TMR0_FREQ);
// Setup the interrupts for the timer timeouts.
IntEnable(INT_TIMER0A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
UARTprintf("Set up timers fini\n");
// Configure les ADC
ConfigureADC();
UARTprintf("Configuration ADC finie\n");
// Enable the timers.
TimerEnable(TIMER0_BASE, TIMER_A);
UARTprintf("Set up fini\n");
// Loop forever while the timers run.
while(1){}
}
The UART send this:
GO!
Set up timers fini
Configuration des ADC
ADC et ports I/O autorisés
Séquenceurs ADC désactivés
Configuration 1 finie
Configuration des ADC finie
Configurations des séquences
Activation des ADC
Configuration ADC finie
Set up fini
Sequence: 1545 1811 1466
Sync.: 1173 1151 1637 1622
Sequence: 1350 1641 1436
Sync.: 989 986 1437 1410
Sequence: 1237 1525 1394
Sync.: 911 888 1320 1286
Sequence: 1141 1434 1340
Sync.: 843 849 1230 1221
Sequence: 1102 1367 1296
Sync.: 816 800 1192 1166
Sequence: 1073 1325 1265
Sync.: 781 773 1145 1141
Sequence: 1051 1294 1238
Sync.: 780 769 1143 1133
Sequence: 1049 1278 1239
Sync.: 785 763 1150 1131
Sequence: 1047 1277 1234
Sync.: 771 754 1131 1114
Sequence: 1041 1265 1226
Sync.: 771 759 1135 1127
Sequence: 1060 1272 1227
Sync.: 773 755 1140 1125
Sequence: 1037 1259 1224
Sync.: 766 760 1130 1109
Sequence: 1037 1265 1223
Sync.: 766 773 1126 1115
Sequence: 1038 1253 1219
Sync.: 765 768 1127 1112
etc...
But if there is no input, it should be:
...
Sequence: 0 0 0
Sync.: 0 0 0 0
Sequence: 0 0 0
Sync.: 0 0 0 0
etc...
So, what am I doing wrong?
Also, considering the frequency (100kHz) that I need to get the data andmake calculations, should I configure it as in the data sheet or the driverlib/adc is ok?
If you have any question, please ask me,
Thank you