Other Parts Discussed in Thread: DRV8301, TMS570LS3137, MOTORWARE
Hi,
About the DRV8301_TMS570LS31_BLDC example.
It seems the data in the graph is not correct. There are some discontinuities in the displayed graph sometimes.
Especially if the prescalar is set to values below 5. I believe it comes from the transmission of the data over usb from the controller to the computer.
And the different graphs do not fit together, The voltage is not in sync with the flux.
So how is this graph-thing and the transmission exactly working? Where can i read about it? Can i make some adjustments, for example buffer size, Speed?
Where is the code? Is it in the InstaSPIN_BLDC.lib?
How can I get the data properly displayed?
Is this a known issue?
My version is CCS 5.3. I cannot use newer versions as I was told. I have tried.