Other Parts Discussed in Thread: RM57L843
Hi,
We are working RM57L843(Rev B) custom based board.
When we are trying to download the code to flash using GHS multi IDE, first memory is copied to RAM and then it will write into flash, but it is failing at the RAM load itself. When we run RAM test from GHS it is failed at starting location itself(at start address itself failing ) not even after at some address location, for flash address locations also same result(unable to write at those locations) and same situation for Flash test also.But we are able to access the core control registers(Like r0,r1,program counter,stack pointer and other processor control registers..etc) and we are able to change those registers and access back changed registers. But after reset when we try to read the RAM and flash locations those values are junk values and no proper sequence is there , and when we try to read System general purpose registers values are junk only except program counter(pc).I am attaching CPU core registers.
Can any one tell me what could be the issue to acess the RAM.Let me know is any others details needed.
Thanks & Regards,