Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
Greetings TI
I have a trouble with the Safety Library code for TMS570LC4357 available in HalCoGen. When I run Selftest for STC1 in Diagnostic mode, the code runs to
Also the STC register Status are
and the status of ESM registers are
As per the explanation in Technical Reference Manual, the test_fail bit has to set in STCGSTAT after the Selftest completion. But it dint happen as expected. The clock being set are GCLK - 300MHz, HCLK - 150MHz, VCLK2 - 75MHz. Please let me know what is the expected behavior after Selftest and why I get this error?
Thanks in advance!