This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where is the Flash State Machine Command Register (FSM_COMMAND) in RM48 and RM57?

Hello

I need to write some specific macro instructions to manage EEPROM in RM48 and RM57.

I have the following documentation:

SPNA148       Advanced F021 Flash API Erase/Program Usage

SPNU501       F021 Flash API Version 2.00.00 Reference Guide

SPNU503B     RM48x 16/32-Bit RISC Flash Microcontroller Technical Reference Manual

SPNU562       RM57Lx 16/32-Bit RISC Flash Microcontroller Technical Reference Manual

In the SPNA148 documentation the command to WRITE / ERASE the EEPROM is in the following register:

FFF8 720C FSM_COMMAND The command to be executed.

I cannot find this register in RM48 or RM578

What is the name of this register in RM48 and RM57?

Thanks for your help

Kind Regards

Jerome

You see below the registers shown by CCS.