This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HalCodeGen (RM48L952ZWT): GMII_SEL

Just out of curiosity, where in PINMUX would I find GMII_SEL?

The EE on the project wrote:

1.3.31. Write 0x01010001 to PINMMR29 at 0xFFFFEB84. This enables SPI2NENA (not used), note that PINMMR29[8] must not be set to enable the EMIF_CLK to the SDRAM, GIOB[2] (PET_WATCHDOG), and GMII_SEL (not used).

I realize that he said that the option is not used, so I do not care about it, but I did not see that on the PINMUX table anywhere, so I was curious.

Also, I did not see EMIF_CLK. He said that I should not enable EMIF_CLK to the SDRAM. I want to make sure that I do not do that, but I do not see that selection anywhere in the PINMUX table