Context : CCS Version 6.0.1.00040 under windows 7/64 - TMDS570LS31HDK
Hello,
When executing some code hosted in the external SDRAM from TMDS570LS31HDK we see a performance drop from a factor 8.3 compared to an execution of the same code in internal flash.
Is this performance drop normal, or do we need to optimize our EMIF settings ?
Is this performance drop only due to EMIF or could it be better if using another type of RAM memory (MRAM instead of SDRAM for example ?)
Thanks for your support,
Regards,
Christophe