I have a circuit board with a TI TM4C123GH6PM processor. I am using the Keil IDE with a ULINK-2 connected to the jtag pins. If I press Debug -> start debug session, I can see my image being dowloaded. Similarly if I press Flash -> Download , I can see my image being downloaded.
When I power off and power on the board with the TM4C123GH6PM the processor appears to be running an older executable image. Is there something I need to do to make my new image be persistemt across power cycles?