This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trip of TMS57LS0432 Hercules launchpad board due to overheating.

Hi,

The above mention TI's launchpad board i am using is now started overheating problem, due to which it is getting tripped off after 30-40 secs.

The heating location is around "TPS70445PWP" voltage regulator in the board.

Could anybody help me out to troubleshoot this issue. I am able to program the board in those 30-40 sec. when it remains ON.

Thanks for the help in advance.

Rahul

  • Hi Rahul,

    Is the overheating just occurring recently? Do you have anything connected to the board right now? If yes, can you disconnect them and see if the overheating subsides? Can you also measure the IO (3.3V) and core (1.2V) voltages at TP1 and TP2 on the board?