Other Parts Discussed in Thread: TMS570LS3137
Hi all,
I have to benchmark a compute intensive application that uses a huge amount of data stored in external SDRAM.
I'm using CCS 6.01.00040 for a TMS570LS3137 rev. C on an Hercules Dev. Kit rev. E; the compiler is ARM 5.1.6.
In evaluating an exponential, I fall into an exception case ; having the exception isn't the problem? It's the raising of the exception that gives a prefetch error. After digging into the issue, I see in the library code an STMIA instruction. Is this instruction subject to the STM/LDM bug too ?
I think this is related to my prefetch issue because since I compile the app with the --no_stm flag, all other prefetch issues I had are gone.
In case of a positive answer to the above question, how can I compile the library with the --no_stm flag ?
I think there is a more recent release of the ARM compiler. Is there a direct link I can use to get it ? What is the install procedure ? I cannot use any updater channel because of WEB access security related restrictions.
Thanks for your answer
Marc