Hello,
I use the TM4C129EXL evaluation kit.
I want to use 4 PWM, 2 couples of PWM with dead band mode. To do so, I use the following code wich configure the pins PF2 and PF3 (module 0 generator 1), and PK4 and PK5 (module 0 generator 3).
I use the code given in the exemple "dead_band.c". I adapted it and it works fine for the couple PF2 and PF3. But with PK4 and PK5, nothing happen. I thought it was a muxing problem sinc PK4 and PK5 are used for the ethernet LED.
Thank you for your help.
Here is the code:
int
main(void)
{
        PinoutSet(false,false);
	SysCtlPWMClockSet(SYSCTL_PWMDIV_1);
	SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	HWREG(GPIO_PORTK_BASE + GPIO_O_CR) = 0x01;
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	HWREG(GPIO_PORTK_BASE + GPIO_O_CR) = 0x02;
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	HWREG(GPIO_PORTK_BASE + GPIO_O_CR) = 0x04;
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	HWREG(GPIO_PORTK_BASE + GPIO_O_CR) = 0x08;
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	GPIOPinConfigure(GPIO_PK4_M0PWM6);
	GPIOPinConfigure(GPIO_PK5_M0PWM7);
	GPIOPinTypePWM(GPIO_PORTK_BASE, GPIO_PIN_4);
	GPIOPinTypePWM(GPIO_PORTK_BASE, GPIO_PIN_5);
	PWMGenConfigure(PWM0_BASE, PWM_GEN_3, PWM_GEN_MODE_UP_DOWN |
			PWM_GEN_MODE_NO_SYNC);
	PWMGenPeriodSet(PWM0_BASE, PWM_GEN_3, 64000);
	PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4,
			PWMGenPeriodGet(PWM0_BASE, PWM_GEN_3) / 4);
	PWMDeadBandEnable(PWM0_BASE, PWM_GEN_3, 160, 160);
	PWMOutputState(PWM0_BASE, PWM_OUT_5_BIT | PWM_OUT_4_BIT, true);
	HWREG(GPIO_PORTK_BASE + GPIO_O_CR) = 0x00;
	HWREG(GPIO_PORTK_BASE + GPIO_O_LOCK) = 0;
//////////////////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////////////////
	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
	GPIOPinConfigure(GPIO_PF2_M0PWM2);
	GPIOPinConfigure(GPIO_PF3_M0PWM3);
	GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_2);
	GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_3);
	PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_UP_DOWN |
			PWM_GEN_MODE_NO_SYNC);
	PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, 1200);
	PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2,
			PWMGenPeriodGet(PWM0_BASE, PWM_GEN_1) / 4);
	PWMDeadBandEnable(PWM0_BASE, PWM_GEN_1, 160, 160);
	PWMOutputState(PWM0_BASE, PWM_OUT_3_BIT | PWM_OUT_2_BIT, true);
	PWMGenEnable(PWM0_BASE, PWM_GEN_1);
	PWMGenEnable(PWM0_BASE, PWM_GEN_3);
	while(1)
	{
	}
}