Dear all,
1.Firstly, I am looking for the PCB(or called Launchpad) has MCU can handle at least 35 ADC at same time. Basically, I have 35 sensor working at same time, I need plug into the ADC input pins. I found LAUNCHXL2-570LC43(MCU:TMS570C4357) & LAUNCHXL2-RM57L(mcu:RM57L843). Am I in the correct direction??
2. I could not find any pin map/connection map for those two board. I am not sure what is the actual layout the PCB
2-1) I found the schematics For LAUNCHXL-570LC43, processors.wiki.ti.com/.../LAUNCHXL2_570LC43_RM57L_SCHEMATICS.pdf. U1A-U1D are standing for what meaning. I just want make sure if I got notification correctly.
2-2) Page 8&7 title "BOOSTER PACK 1/2". I know it help to develop. But what is really it? Are they add-ons? Do I have to purchase the booster pack in order to access the pins? I need 35 input pins, lots of wires to connect.
3. RM57L and 570LC43 share the same schematics? The ti.wiki link is the same page. The pcb is EXACTLY same pin layout? I am assuming they use different MCU, should not be different layout?
4. I also found datasheet LAUNCHXL2-RM57L( user manual) in Development kit :www.ti.com/.../spnu598.pdf.
The board color is GREEN, it is not red base color as shown in product list. I am so confusing now.
4-1)Is this board I am going to get?
4-2)Or the Red board?
4-3) Should I follow the schematics? or the user manual of development kit?
5. What is different between development kit and Evaluation Kit ?
I got lots of boring questions. Thanks for your time.