This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt SSI



Hi, I am  not understand SSI interrupt to send char or array of char

Now  I create system in tm4c1294 and use leds for indicate interrupt flags, and in interrupt handler clear it, but it not reset.

init ssi function

void SSI3_TI_init(void)
{
     SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
         
     SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
    
     GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
     GPIOPinConfigure(GPIO_PQ1_SSI3FSS);
     GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);
     GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);
    
     GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 |GPIO_PIN_0);
    
      IntMasterEnable();
 
     SSIConfigSetExpClk(SSI3_BASE, 48000000, SSI_FRF_TI, SSI_MODE_MASTER, 2000000, 8);
    
     SSIIntRegister(SSI3_BASE, SSI3_Int_Handler);
    
     SSIIntEnable(SSI3_BASE, SSI_TXEOT|SSI_RXFF);//SSI_RXTO|SSI_RXOR|SSI_TXFF
        
     IntEnable(INT_SSI3);
        
     SSIEnable(SSI3_BASE);
}

send func

void send_byte_ssi3 (uint32_t value)
{
    while ( ((SSIIntStatus(SSI3_BASE, true)) & SSI_TXFF) == 0 );
        SSIDataPut(SSI3_BASE, value );
}

interrupt handler

void SSI3_Int_Handler(void)
{
    
     uint32_t ui32Status;

    //
    // Read the interrupt status to find the cause of the interrupt
    //
   ui32Status = SSIIntStatus(SSI3_BASE, true);
        if (ui32Status & SSI_TXEOT)
        {
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
            SSIIntClear (SSI3_BASE, SSI_TXEOT);
        }
        if (ui32Status & SSI_TXFF)
        {
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, GPIO_PIN_1);
            SSIIntClear (SSI3_BASE, SSI_TXFF);
            if(((SSIIntStatus(SSI3_BASE, true)) && SSI_TXFF) == 0)
            {
                GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, GPIO_PIN_0);
            }
            else
            {
                GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, GPIO_PIN_4);
            }
                
        }
   
}

main

int main(void)
{
    uint32_t pui32DataTx[NUM_SSI_DATA];
    uint32_t pui32DataRx[NUM_SSI_DATA];
    uint32_t ui32Index;

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                   SYSCTL_XTAL_16MHZ);

    InitConsole();

    UARTprintf("SSI ->\n");
    UARTprintf("  Mode: TI\n");
    UARTprintf("  Data: 8-bit\n\n");
    
    
        board_leds_ini();
    
      SSI3_TI_init();
        
      //
    // Initialize the data to send.
    //
    pui32DataTx[0] = 't';
    pui32DataTx[1] = 'i';
    pui32DataTx[2] = '!';

    //
    // Display indication that the SSI is transmitting data.
    //
    UARTprintf("Sent:\n  ");

    //
    // Send 3 bytes of data.
    //
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        //
        // Display the data that SSI is transferring.
        //
        UARTprintf("'%c' ", pui32DataTx[ui32Index]);

        //
        // Send the data using the "blocking" put function.  This function
        // will wait until there is room in the send FIFO before returning.
        // This allows you to assure that all the data you send makes it into
        // the send FIFO.
        //
        send_byte_ssi3( pui32DataTx[ui32Index]);
    }

    //
    // Wait until SSI0 is done transferring all the data in the transmit FIFO.
    //
    while(SSIBusy(SSI3_BASE))
    {
    }

    //
    // Display indication that the SSI is receiving data.
    //
    UARTprintf("\nReceived:\n  ");

    //
    // Receive 3 bytes of data.
    //
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        //
        // Receive the data using the "blocking" Get function. This function
        // will wait until there is data in the receive FIFO before returning.
        //
        SSIDataGet(SSI3_BASE, &pui32DataRx[ui32Index]);

        //
        // Since we are using 8-bit data, mask off the MSB.
        //
        pui32DataRx[ui32Index] &= 0x00FF;

        //
        // Display the data that SSI0 received.
        //
        UARTprintf("'%c' ", pui32DataRx[ui32Index]);
    }
        UARTprintf("\n ");
    //
    // Return no errors
    //
    return(0);
}

In result I am not have SSI_TXEOT bit set, and not received information, bit SSI_TXFF but not work

Ps Thanks for all answers