This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use secondary uDMA channel (ADC1)



Hi all,

I'm making an oscilloscope which acquires data from 2 channels, and I'm transferring data to memory using uDMA. I have decided to use uDMA channels ADC1 and ADC0 for this.

I have already made a working ping pong uDMA transfer using UDMA_CHANNEL_ADC0; however, I can't seem to get UDMA_SEC_CHANNEL_ADC10 to work at all.

I have used:

uDMAChannelSelectSecondary(UDMA_DEF_SSI1RX_SEC_ADC10);

But I'm not sure if that's all I need to do in order to use UDMA_SEC_CHANNEL_ADC10.

I've attached my code below.

Any help would be much appreciated. Thank you in advance.

/* ----------------------------------------------------------------------------
 * Includes
 * ------------------------------------------------------------------------- */

#include <stdint.h>
#include <stdbool.h>

/* Tivaware Header files */
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "inc/hw_adc.h"
#include "driverlib/timer.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h"
#include "driverlib/udma.h"

/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>

#include "adc.h"

/* ----------------------------------------------------------------------------
 * Defines
 * ------------------------------------------------------------------------- */

#define DEBUG_LED
//#define DEBUG_DMA

/* ----------------------------------------------------------------------------
 * External variables
 * ------------------------------------------------------------------------- */

	// Samples buffer for both channels
uint16_t pui16SamplesA[MAX_NUM_SAMPLES + DMA_TRANSFER_SIZE];
uint16_t pui16SamplesB[MAX_NUM_SAMPLES + DMA_TRANSFER_SIZE];

	// Flag to indicate sampling done
uint8_t ui8DoneA;
uint8_t ui8DoneB;

uint16_t ui16TriggerPointA;

/* ----------------------------------------------------------------------------
 * Private variables
 * ------------------------------------------------------------------------- */

	// Number of transfers required to obtain desired number of samples
static uint8_t ui8DMATransfers;

	// DMA transfer destinations
static uint16_t *pui16DMADestA;
static uint16_t *pui16DMADestB;

	// Comparator levels for triggering
	// [CHANNEL (CHAN_A, CHAN_B)][BOUNDARY (HIGH, LOW)]
static uint16_t pui16ComparatorLevels[2][2];

	// Triggering utilities
static volatile uint16_t ui16SamplesTracker;
static volatile uint8_t ui8Triggered;
static volatile uint16_t ui16SamplesTakenAfterTrigger;

	// uDMA control table
static uint8_t pui8DMAControlTable[1024];

/* ----------------------------------------------------------------------------
 * Private Functions
 * ------------------------------------------------------------------------- */

/*
 * @brief	Modifies the uDMA destination address to point to the next block
 * 			to be written to.
 * @params	The channel destination address to be changed
 * @retval	None
 */
static void
advance_dma_dest(uint8_t channel) {

	//
	// Increment the destination address by the uDMA transfer size.
	// When the address goes beyond the required nunber of samples,
	// have the address point to the start of the samples buffer.
	//
	switch (channel) {
	case CHAN_A:
		pui16DMADestA += DMA_TRANSFER_SIZE;
		if (pui16DMADestA >=
			(pui16SamplesA + (DMA_TRANSFER_SIZE * ui8DMATransfers))) {
			// Destination at end of buffer, point to start now
			pui16DMADestA = pui16SamplesA;
		}
		break;
	case CHAN_B:
		pui16DMADestB += DMA_TRANSFER_SIZE;
		if (pui16DMADestB >=
			(pui16SamplesB + (DMA_TRANSFER_SIZE * ui8DMATransfers))) {
			// Destination at end of buffer, point to start now
			pui16DMADestB = pui16SamplesB;
		}
		break;
	}
}

/*
 * @brief	Interrupt handler for the ADC timer timeout. Used to keep track of
 * 			the number of samples taken after trigger, and where the latest
 * 			sample is at in the buffer.
 * @params	None
 * @retval	None
 */
void
adc_timer_irq(void) {

	// Clear interrupt
	TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);

	// Cycle the samples buffer trackers
	ui16SamplesTracker++;
	ui16SamplesTracker %= (DMA_TRANSFER_SIZE * ui8DMATransfers);

	// Count samples taken after trigger
	if (ui8Triggered) {
		ui16SamplesTakenAfterTrigger++;
	}
}

/*
 * @brief	Helper function to test if a short is within a boundary.
 * @params	Test value, low and high boundaries
 * @retval	1 if test value is within boundaries
 * 			0 if test value is not within boundaries
 */
static int
is_within(uint16_t test, uint16_t low, uint16_t high) {

	if (test > high) {
		return 0;
	}
	if (test < low) {
		return 0;
	}
	return 1;
}

/*
 * @brief	Comparator interrupt for channel A. Stores triggering point, and
 * 			flips the ui8Triggered flag.
 * @params	None
 * @retval	None
 */
void adc_A_comp_irq(void) {

	uint16_t ui16TestSample;

	// Clear comparator interrupt
	ADCComparatorIntClear(ADC0_BASE, ADC_DCISC_DCINT0 | ADC_DCISC_DCINT1);

	//
	// Check that the current analog signal is near the comparator boundaries
	// If the signal is not, then this is a false trigger, return immediately
	//
	ui16TestSample = *(uint16_t *) (ADC0_BASE + ADC_O_SSFIFO0);
	if (!is_within(ui16TestSample,
				pui16ComparatorLevels[CHAN_A][LOW] - COMP_TOLERANCE,
				pui16ComparatorLevels[CHAN_A][LOW] + COMP_TOLERANCE)
			&&
		!is_within(ui16TestSample,
				pui16ComparatorLevels[CHAN_A][HIGH] - COMP_TOLERANCE,
				pui16ComparatorLevels[CHAN_A][HIGH] + COMP_TOLERANCE)
		)
		return;

#ifdef DEBUG_LED

	static uint16_t i = 1;

	// Toggle GPIO pin for every valid trigger
	if (i++ % 2) {
		GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_PIN_4);
	} else {
		GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_4, 0);
	}

#endif

	// Store the triggering point, and flip the triggered flag
	ui16TriggerPointA = ui16SamplesTracker;
	ui8Triggered = 1;

	// Disable comparator interrupt. Reenabled when sampling begins again.
	IntDisable(INT_ADC0SS1);
	IntDisable(INT_ADC1SS1);
}

/*
 * @brief	Comparator interrupt for channel B. Stores triggering point, and
 * 			flips the ui8Triggered flag.
 * @params	None
 * @retval	None
 */
void adc_B_comp_irq(void) {

	// Clear comparator interrupt
	ADCComparatorIntClear(ADC1_BASE, ADC_DCISC_DCINT2 | ADC_DCISC_DCINT3);
}




void adc_A_dma_irq(void) {

	uint32_t modePrimary;
	uint32_t modeAlternate;

	// Clear ADC uDMA interrupt
	ADCIntClearEx(ADC0_BASE, ADC_INT_DMA_SS0);

	// Get mode statuses
	modePrimary 	= uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT);
	modeAlternate 	= uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT);

	// Reload the control structures
	if ((modePrimary == UDMA_MODE_STOP) && (modeAlternate != UDMA_MODE_STOP)) {

		// Need to reload primary control structure
		uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
								UDMA_MODE_PINGPONG,
								(void *) (ADC0_BASE + ADC_O_SSFIFO0),
								pui16DMADestA,
								DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_A);

	} else if ((modePrimary != UDMA_MODE_STOP)
			&& (modeAlternate == UDMA_MODE_STOP)) {

		// Need to reload alternate control structure
		uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
								UDMA_MODE_PINGPONG,
								(void *) (ADC0_BASE + ADC_O_SSFIFO0),
								pui16DMADestA,
								DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_A);

	} else {
		// Either both still not stopped, or both stopped. This is an error
#ifdef DEBUG_DMA
		System_printf("Error in uDMA control structure modes\n");
		System_printf("Primary mode: %d\nAlternate mode: %d\n", modePrimary,
				modeAlternate);
		System_printf(
				"For reference: Stop:%d, Basic:%d, Auto:%d, PingPong:%d, MemScatter:%d, PerScatter:%d\n",
				UDMA_MODE_STOP, UDMA_MODE_BASIC, UDMA_MODE_AUTO,
				UDMA_MODE_PINGPONG, UDMA_MODE_MEM_SCATTER_GATHER,
				UDMA_MODE_PER_SCATTER_GATHER);
		System_flush();
#endif
	}

	// TODO: MOdify so that sampling only stops when both channels are done

	// Stop udma if we have triggered, and obtained the correct amount of samples
	if (ui16SamplesTakenAfterTrigger
			>= (DMA_TRANSFER_SIZE * ui8DMATransfers / 2)) {
		ui8DoneA = 1;
		ui8DoneB = 1;
	}

	if (ui8DoneA && ui8DoneB) {
		sampling_stop();
	}
}

void adc_B_dma_irq(void) {

	uint32_t modePrimary;
	uint32_t modeAlternate;

	// Clear ADC uDMA interrupt
	ADCIntClearEx(ADC1_BASE, ADC_INT_DMA_SS0);

	// Get mode statuses
	modePrimary 	= uDMAChannelModeGet(UDMA_SEC_CHANNEL_ADC10 | UDMA_PRI_SELECT);
	modeAlternate 	= uDMAChannelModeGet(UDMA_SEC_CHANNEL_ADC10 | UDMA_ALT_SELECT);

	// Reload the control structures
	if ((modePrimary == UDMA_MODE_STOP) && (modeAlternate != UDMA_MODE_STOP)) {

		// Need to reload primary control structure
		uDMAChannelTransferSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_PRI_SELECT,
								UDMA_MODE_PINGPONG,
								(void *) (ADC1_BASE + ADC_O_SSFIFO0),
								pui16DMADestB,
								DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_B);

	} else if ((modePrimary != UDMA_MODE_STOP)
			&& (modeAlternate == UDMA_MODE_STOP)) {

		// Need to reload alternate control structure
		uDMAChannelTransferSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_ALT_SELECT,
								UDMA_MODE_PINGPONG,
								(void *) (ADC1_BASE + ADC_O_SSFIFO0),
								pui16DMADestB,
								DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_B);

	} else {
		// Either both still not stopped, or both stopped. This is an error
#ifdef DEBUG_DMA
		System_printf("Error in uDMA control structure modes\n");
		System_printf("Primary mode: %d\nAlternate mode: %d\n", modePrimary,
				modeAlternate);
		System_printf(
				"For reference: Stop:%d, Basic:%d, Auto:%d, PingPong:%d, MemScatter:%d, PerScatter:%d\n",
				UDMA_MODE_STOP, UDMA_MODE_BASIC, UDMA_MODE_AUTO,
				UDMA_MODE_PINGPONG, UDMA_MODE_MEM_SCATTER_GATHER,
				UDMA_MODE_PER_SCATTER_GATHER);
		System_flush();
#endif
	}

	// TODO: MOdify so that sampling only stops when both channels are done

	// Stop udma if we have triggered, and obtained the correct amount of samples
	if (ui16SamplesTakenAfterTrigger
			>= (DMA_TRANSFER_SIZE * ui8DMATransfers / 2)) {
		ui8DoneB = 1;
	}

	if (ui8DoneA && ui8DoneB) {
		sampling_stop();
	}
}

/*
 * ========== adc_trigger_timer_init ==========
 * @brief	Initializes the timer for triggering ADC samples
 */
void adc_trigger_timer_init(uint32_t ui32ClockFreq, uint32_t ui32SampleFreq) {

	// Enable timer peripheral clock
	SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER1)) {
	}

	// Register interrupt
	TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
	IntRegister(INT_TIMER1A, adc_timer_irq);
	IntEnable(INT_TIMER1A);

	TimerConfigure(TIMER1_BASE, TIMER_CFG_A_PERIODIC_UP);
	TimerLoadSet(TIMER1_BASE, TIMER_A, (ui32ClockFreq / ui32SampleFreq));
	TimerControlTrigger(TIMER1_BASE, TIMER_A, true);
	TimerADCEventSet(TIMER1_BASE, TIMER_ADC_TIMEOUT_A);
	TimerEnable(TIMER1_BASE, TIMER_A);
}

void comparator_levels_set(uint16_t low, uint16_t high, uint8_t channel) {

	pui16ComparatorLevels[channel][LOW] = low;
	pui16ComparatorLevels[channel][HIGH] = high;

	switch (channel) {
	case CHAN_A:
		ADCComparatorConfigure(ADC0_BASE, 0, ADC_COMP_INT_LOW_HONCE);
		ADCComparatorConfigure(ADC0_BASE, 1, ADC_COMP_INT_HIGH_HONCE);
		ADCComparatorRegionSet(ADC0_BASE, 0, low, high);
		ADCComparatorRegionSet(ADC0_BASE, 1, low, high);

		break;
	case CHAN_B:
		ADCComparatorConfigure(ADC1_BASE, 2, ADC_COMP_INT_LOW_HONCE);
		ADCComparatorConfigure(ADC1_BASE, 3, ADC_COMP_INT_HIGH_HONCE);
		ADCComparatorRegionSet(ADC1_BASE, 2, low, high);
		ADCComparatorRegionSet(ADC1_BASE, 3, low, high);
		break;
	}
}

uint16_t comparator_level_get(uint8_t region, uint8_t channel) {
	return pui16ComparatorLevels[channel][region];
}

/*
 * ========== adc_init ==========
 * @brief	Initializes ADCs for both channels A and B
 */
void adc_init(void) {

	/*
	 * Channel A:
	 * ADC0
	 * Sequencer 0, Step 0 - Sample and uDMA
	 * Sequencer 1, Step 0 - Falling edge trigger (CMP0)
	 * Sequencer 1, Step 1 - Rising edge trigger (CMP1)
	 * Pin PE5 (Channel A8)
	 *
	 * Channel B:
	 * ADC1
	 * Sequencer 0, Step 0 - Sample and uDMA
	 * Sequencer 1, Step 0 - Falling edge trigger (CMP2)
	 * Sequencer 1, Step 1 - Rising edge trigger (CMP3)
	 * Pin PE4 (Channel A9)
	 */

	// Enable GPIO peripheral clock for the ADC input
	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
	SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE)) {
	}
	// Enable ADC peripheral clock
	SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
	SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0)) {
	}
	SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
	SysCtlPeripheralReset(SYSCTL_PERIPH_ADC1);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_ADC1)) {
	}

	// Configure GPIO pins as ADC inputs
	GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4);
	GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_5);

	// Disable interrupts
	ADCIntDisableEx(ADC0_BASE, ADC_INT_DMA_SS0 | ADC_INT_DCON_SS1);
	ADCIntDisableEx(ADC1_BASE, ADC_INT_DMA_SS0 | ADC_INT_DCON_SS1);

	// Disable sequences
	ADCSequenceDisable(ADC0_BASE, 0);
	ADCSequenceDisable(ADC0_BASE, 1);
	ADCSequenceDisable(ADC1_BASE, 0);
	ADCSequenceDisable(ADC1_BASE, 1);

	// Configure the steps of each sequencer
	// Channel A
	ADCSequenceStepConfigure(ADC0_BASE, 0, 0,
	ADC_CTL_CH8 | ADC_CTL_END | ADC_CTL_IE);
	ADCSequenceStepConfigure(ADC0_BASE, 1, 0,
	ADC_CTL_CH8 | ADC_CTL_CMP0 | ADC_CTL_IE);
	ADCSequenceStepConfigure(ADC0_BASE, 1, 1,
	ADC_CTL_CH8 | ADC_CTL_CMP1 | ADC_CTL_END | ADC_CTL_IE);
	// Channel B
	ADCSequenceStepConfigure(ADC1_BASE, 0, 0,
	ADC_CTL_CH9 | ADC_CTL_END | ADC_CTL_IE);
	ADCSequenceStepConfigure(ADC1_BASE, 1, 0,
	ADC_CTL_CH9 | ADC_CTL_CMP2 | ADC_CTL_IE);
	ADCSequenceStepConfigure(ADC1_BASE, 1, 1,
	ADC_CTL_CH9 | ADC_CTL_CMP3 | ADC_CTL_END | ADC_CTL_IE);

	// Configure to use internal 3V reference
	ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
	ADCReferenceSet(ADC1_BASE, ADC_REF_INT);

	// Configure ADC comparators
	comparator_levels_set(COMP_DEFAULT_LOW, COMP_DEFAULT_HIGH, CHAN_A);
	comparator_levels_set(COMP_DEFAULT_LOW, COMP_DEFAULT_HIGH, CHAN_B);

	// TODO
	ADCComparatorReset(ADC0_BASE, 0, true, true);
	ADCComparatorReset(ADC0_BASE, 1, true, true);

	// Enable ADC interrupts for uDMA transfer completion,
	// and digital comparator
	ADCIntEnableEx(ADC0_BASE, ADC_INT_DMA_SS0 | ADC_INT_DCON_SS1);
	ADCIntEnableEx(ADC1_BASE, ADC_INT_DMA_SS0 | ADC_INT_DCON_SS1);

	// Register interrupts
	IntRegister(INT_ADC0SS1, adc_A_comp_irq);
	IntRegister(INT_ADC1SS1, adc_B_comp_irq);
	IntRegister(INT_ADC0SS0, adc_A_dma_irq);
	IntRegister(INT_ADC1SS0, adc_B_dma_irq);

	// Enable interrupts
	IntEnable(INT_ADC0SS0);
	IntEnable(INT_ADC1SS0);

	// Enable ADC to use uDMA
	ADCSequenceDMAEnable(ADC0_BASE, 0);
	ADCSequenceDMAEnable(ADC1_BASE, 0);

	// Enable ADC sequencers
	ADCSequenceEnable(ADC0_BASE, 0);
	ADCSequenceEnable(ADC0_BASE, 1);
	ADCSequenceEnable(ADC1_BASE, 0);
	ADCSequenceEnable(ADC1_BASE, 1);

	// Configure the trigger sources and priorities
	// All sequencers are set to be triggered by timer
	// Sequence 0 has higher priorty (priority 0) than sequence 1 (priority 1)
	ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_TIMER, 0);
	ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_TIMER, 1);
	ADCSequenceConfigure(ADC1_BASE, 0, ADC_TRIGGER_TIMER, 0);
	ADCSequenceConfigure(ADC1_BASE, 1, ADC_TRIGGER_TIMER, 1);
}

/*
 * @params	Number of transfers required to obtain requires number of samples
 */
void dma_start(uint8_t ui8NumTransfers, uint8_t channel) {

	switch (channel) {
	case CHAN_A:
		// Disable before configure
		uDMAChannelDisable(UDMA_CHANNEL_ADC0);
		uDMAChannelDisable(UDMA_SEC_CHANNEL_ADC10);

		// Set the number of transfers
		ui8DMATransfers = ui8NumTransfers;

		// Reset the destination pointer to start of buffer
		pui16DMADestA = pui16SamplesA;
		pui16DMADestB = pui16SamplesB;

		// Configure the transfer parameters
		uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
		UDMA_MODE_PINGPONG, (void *) (ADC0_BASE + ADC_O_SSFIFO0), pui16DMADestA,
		DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_A);

		uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
		UDMA_MODE_PINGPONG, (void *) (ADC0_BASE + ADC_O_SSFIFO0), pui16DMADestA,
		DMA_TRANSFER_SIZE);
		advance_dma_dest(CHAN_A);


		uDMAChannelTransferSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_PRI_SELECT,
				UDMA_MODE_PINGPONG, (void *) (ADC1_BASE + ADC_O_SSFIFO0), pui16DMADestB,
				DMA_TRANSFER_SIZE);
				advance_dma_dest(CHAN_B);

				uDMAChannelTransferSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_ALT_SELECT,
				UDMA_MODE_PINGPONG, (void *) (ADC1_BASE + ADC_O_SSFIFO0), pui16DMADestB,
				DMA_TRANSFER_SIZE);
				advance_dma_dest(CHAN_B);


		uDMAChannelEnable(UDMA_CHANNEL_ADC0);
		uDMAChannelEnable(UDMA_SEC_CHANNEL_ADC10);


		break;
	}
}

void dma_init(void) {

	SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_UDMA)) {
	}

	// Enable uDMA
	uDMAEnable();

	uDMAChannelSelectSecondary(UDMA_DEF_SSI1RX_SEC_ADC10);

	// Set the control table for uDMA
	uDMAControlBaseSet(&pui8DMAControlTable[0]);

	// Disable unneeded attributes of the uDMA channels
	uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0, UDMA_ATTR_ALL);
	uDMAChannelAttributeDisable(UDMA_SEC_CHANNEL_ADC10, UDMA_ATTR_ALL);

	// Channel A
	uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
	UDMA_SIZE_16 |
	UDMA_SRC_INC_NONE |
	UDMA_DST_INC_16 |
	UDMA_ARB_1);
	uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
	UDMA_SIZE_16 |
	UDMA_SRC_INC_NONE |
	UDMA_DST_INC_16 |
	UDMA_ARB_1);


	// Channel B
	uDMAChannelControlSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_PRI_SELECT,
	UDMA_SIZE_16 |
	UDMA_SRC_INC_NONE |
	UDMA_DST_INC_16 |
	UDMA_ARB_1);
	uDMAChannelControlSet(UDMA_SEC_CHANNEL_ADC10 | UDMA_ALT_SELECT,
	UDMA_SIZE_16 |
	UDMA_SRC_INC_NONE |
	UDMA_DST_INC_16 |
	UDMA_ARB_1);
}

void sampling_start(uint16_t numSamples, uint32_t clockFreq,
		uint32_t samplingFreq) {

	ui16SamplesTracker 				= 0;
	ui8Triggered 					= 0;
	ui8DoneA 						= 0;
	ui8DoneB						= 0;
	ui16SamplesTakenAfterTrigger 	= 0;

	ui16TriggerPointA = 0;

#ifdef DEBUG_LED

	// Enable Port C
	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
	while (!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOC)) {
	}
	// Set C4 to be output
	GPIOPinTypeGPIOOutput(GPIO_PORTC_BASE, GPIO_PIN_4);

#endif

	dma_init();
	dma_start((numSamples / DMA_TRANSFER_SIZE), CHAN_A);
	adc_init();
	adc_trigger_timer_init(clockFreq, samplingFreq);

	Task_sleep(10);
	IntEnable(INT_ADC0SS1);
	IntEnable(INT_ADC1SS1);

}

// TODO: not channel independent
void sampling_stop() {


	IntDisable(INT_ADC0SS0);
	IntDisable(INT_ADC1SS0);

	uDMAChannelDisable(UDMA_CHANNEL_ADC0);
	uDMAChannelDisable(UDMA_SEC_CHANNEL_ADC10);

	TimerDisable(TIMER1_BASE, TIMER_A);

	ADCSequenceDisable(ADC0_BASE, 0);
	ADCSequenceDisable(ADC1_BASE, 0);

}

  • The API "uDMAChannelSelectSecondary" is old and has been replaced with the API "uDMAChannelAssign". Please use this new API.

    Also the mapping "UDMA_SEC_CHANNEL_ADC10 " is replaced with a new mapping (for the API "uDMAChannelAssign"). These new mappings are present in the file "udma.h". If using uDMA Channel 24 for ADC1 SS0, the parameter to be passed to the API "uDMAChannelAssign" is "UDMA_CH24_ADC1_0".

    Thanks,
    Sai